This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad9081_fmca_ebz:ad9081_fmca_ebz_hdl [07 Apr 2021 07:07] – [Example block design for Single Link; M=2; L=8; JESD204C] Laszlo Nagy | resources:eval:user-guides:ad9081_fmca_ebz:ad9081_fmca_ebz_hdl [14 Jun 2021 07:37] – [Example block design for Single Link; M=2; L=8; JESD204C] Laszlo Nagy | ||
---|---|---|---|
Line 49: | Line 49: | ||
# Parameter description: | # Parameter description: | ||
# JESD_MODE : used link layer encoder mode | # JESD_MODE : used link layer encoder mode | ||
- | # 64B66B - 64b66b link layer defined in JESD 204C, uses Xilinx IP as Physical layer | + | # 64B66B - 64b66b link layer defined in JESD 204C |
- | # 8B10B - 8b10b link layer defined in JESD 204B, uses ADI IP as Physical layer | + | # 8B10B - 8b10b link layer defined in JESD 204B |
# | # | ||
- | # RX_RATE : line rate of the Rx link ( MxFE to FPGA ) used in 64B66B mode | + | # RX_RATE : line rate of the Rx link ( MxFE to FPGA ) |
- | # TX_RATE : line rate of the Tx link ( FPGA to MxFE ) used in 64B66B mode | + | # TX_RATE : line rate of the Tx link ( FPGA to MxFE ) |
- | # REF_CLK_RATE : frequency of reference clock in MHz used in 64B66B mode | + | |
# [RX/ | # [RX/ | ||
# [RX/ | # [RX/ | ||
Line 78: | Line 77: | ||
* NP = 8, 12, 16 | * NP = 8, 12, 16 | ||
- | * F = 1, 2, 3, 4, 6 | + | * F = 1, 2, 3, 4, 6, 8 |
* https:// | * https:// | ||
* https:// | * https:// | ||
Line 145: | Line 144: | ||
==== Example block design for Single Link; M=2; L=8; JESD204C ==== | ==== Example block design for Single Link; M=2; L=8; JESD204C ==== | ||
+ | |||
+ | Observation: | ||
{{ : | {{ : | ||
Line 178: | Line 179: | ||
* REF_CLK – 500 MHz (Lane Rate/33) | * REF_CLK – 500 MHz (Lane Rate/33) | ||
* JESD204C Lane Rate – 16.5Gbps | * JESD204C Lane Rate – 16.5Gbps | ||
- | * QPLL1 - selected in Xilinx PHY | + | * QPLL1 |
The Tx link is operating with the following parameters: | The Tx link is operating with the following parameters: | ||
Line 187: | Line 188: | ||
* REF_CLK – 500 MHz (Lane Rate/33) | * REF_CLK – 500 MHz (Lane Rate/33) | ||
* JESD204C Lane Rate – 16.5Gbps | * JESD204C Lane Rate – 16.5Gbps | ||
- | * QPLL1 - selected in Xilinx PHY | + | * QPLL1 |
===== Clock sources ===== | ===== Clock sources ===== |