The AD7768-1 is a low power, high performance, Σ-Δ analog-to-digital converter (ADC), with a Σ-Δ modulator and digital filter for precision conversion of both ac and dc signals. The AD7768-1 is a single channel version of the AD7768, an 8-channel, simultaneously sampling, Σ-Δ ADC. The AD7768-1 provides a single configurable and reusable data acquisition footprint, which establishes a new industry standard in combined ac and dc performance and enables instrumentation and industrial system designers to design across multiple measurement variants for both isolated and nonisolated applications.
The AD7768-1 achieves a 108.5 dB dynamic range when using the low ripple, finite impulse response (FIR) digital filter at 256 kSPS, giving 110.8 kHz input bandwidth (BW), combined with ±1.1 ppm integral nonlinearity (INL), ±30 µV offset error, and ±30 ppm gain error.
Wider bandwidth, up to 500 kHz Nyquist, 204 kHz, −3 dB, is available using the sinc5 filter, enabling a view of signals over an extended range.
The AD7768-1 offers the user the flexibility to configure and optimize for input BW vs. output data rate (ODR) and vs. power dissipation. The flexibility of the AD7768-1 allows for dynamic analysis of a changing input signal, making it particularly useful in general-purpose data acquisition systems. The selection of one of three available power modes allows the designer to achieve required noise targets while minimizing power consumption. The design of the AD7768-1 is unique in that it becomes a reusable and flexible platform for low power dc and high performance ac measurement modules.
The AD7768-1 achieves the optimum balance of dc and ac performance with excellent power efficiency. The following three operating modes allow the user to tailor the input BW vs. power budgets:
The AD7768-1 offers extensive digital filtering capabilities that can meet a wide range of system requirements. The filter options allow configuration for frequency domain measurements with tight gain error over frequency, linear phase response requirements (brick wall filter), a lower latency path (sinc5 or sinc3) for use in control loop applications, and measuring dc inputs with the ability to configure the sinc3 filter to reject the line frequency of either 50 Hz or 60 Hz. All filters offer programmable decimation.
A 1.024 MHz sinc5 filter path exists for users seeking an even higher output data rate. This path is quantization noise limited; therefore, it is best suited for customers requiring minimum latency for control loops or implementing custom digital filtering on an external field programmable gate array (FPGA) or digital signal processor (DSP).
Filter options include the following:
When using the AD7768-1, embedded analog functionality within the AD7768-1 greatly reduces the design burden over the entire application range. The precharge buffer on each analog input decreases analog input current compared to competitive offerings, simplifying the task of an external amplifier to drive the analog input.
A full buffer input on the reference vastly reduces the input current, providing a high impedance input for the external reference device or in buffering any reference sense resistor scenarios used in ratiometric measurements.
The device operates with a 5.0 V AVDD1 − AVSS supply, a 2.0 V to 5.0 V AVDD2 − AVSS supply, and a 1.8 V to 3.3 V IOVDD − DGND supply.
In low power mode, the AVDD1, AVDD2, and IOVDD supplies can run from a single 3.3 V rail.
The device requires an external reference; the absolute input reference (REFIN) voltage range is 1 V to AVDD1 − AVSS.
The specified operating temperature range is −40°C to +125°C. The device is housed in a 4 mm × 5 mm, 28-lead LFCSP.
In the ADI Reference Designs HDL User Guide can be found an in-depth presentation and instructions about the HDL design in general.
The reference design uses the standard SPI Engine Framework, the offload module is triggered by the DRDY (data ready) signal of the device. Because the board has two AD7768-1, the data path consists of two separate SPI interface and GPIOs, and two DMAs for data stream capture.
In order to build the HDL design the user has to go through the following steps:
Function | Description |
---|---|
int32_t ad77681_setup(ad77681_dev **device, ad77681_init_param init_param); | Initialize the device. |
int32_t ad77681_soft_reset(ad77681_dev *dev); | Device reset over SPI. |
int32_t ad77681_set_status_bit(ad77681_dev *dev, bool status_bit); | Enables Status bits output. |
int32_t ad77681_set_crc_sel(ad77681_dev *dev, ad77681_crc_sel crc_sel); | Activates CRC on all SPI transactions and Selects CRC method as XOR or 8-bit polynomial. |
int32_t ad77681_set_convlen(ad77681_dev *dev, ad77681_conv_len conv_len); | Set the Conversion Result Output Length. |
int32_t ad77681_set_conv_mode(ad77681_dev *dev, ad77681_conv_mode conv_mode, ad77681_conv_diag_mux diag_mux_sel, bool conv_diag_sel); | Conversion mode and source select. |
int32_t ad77681_set_mclk_div(ad77681_dev *dev, ad77681_mclk_div clk_div); | Set the MCLK divider. |
int32_t ad77681_set_power_mode(ad77681_dev *dev, ad77681_power_mode mode); | Set the power consumption mode of the ADC core. |
int32_t ad77681_spi_read_adc_data(ad77681_dev *dev, uint8_t *adc_data); | Read conversion result from device. |
int32_t ad77681_spi_write_mask(ad77681_dev *dev, uint8_t reg_addr, uint8_t mask, uint8_t data); | SPI write to device using a mask. |
int32_t ad77681_spi_read_mask(ad77681_dev *dev, uint8_t reg_addr, uint8_t mask, uint8_t *data); | SPI read from device using a mask. |
int32_t ad77681_spi_reg_read(ad77681_dev *dev, uint8_t reg_addr, uint8_t *reg_data); | Read from device. |
int32_t ad77681_compute_xor(uint8_t *data, uint8_t data_size); | Compute XOR checksum. |
int32_t ad77681_compute_crc8(uint8_t *data, uint8_t data_size); | Compute CRC8 checksum. |
typedef enum { AD77681_ECO = 0, AD77681_MEDIAN = 2, AD77681_FAST = 3, } ad77681_power_mode; typedef enum { AD77681_MCLK_DIV_16 = 0, AD77681_MCLK_DIV_8 = 1, AD77681_MCLK_DIV_4 = 2, AD77681_MCLK_DIV_2 = 3 } ad77681_mclk_div; typedef enum { AD77681_CONV_CONTINUOUS = 0, AD77681_CONV_ONE_SHOT = 1, AD77681_CONV_SINGLE = 2, AD77681_CONV_PERIODIC = 3 } ad77681_conv_mode; typedef enum { AD77681_CONV_24BIT = 0, AD77681_CONV_16BIT = 1 } ad77681_conv_len; typedef enum { AD77681_RDY_DOUT_EN, AD77681_RDY_DOUT_DIS } ad77681_rdy_dout; typedef enum { AD77681_TEMP_SENSOR = 0x0, AD77681_AIN_SHORT= 0x8, AD77681_POSITIVE_FS = 0x9, AD77681_NEGATIVE_FS = 0xA } ad77681_conv_diag_mux; typedef enum { AD77681_CRC, AD77681_XOR, AD77681_NO_CRC } ad77681_crc_sel; typedef struct { /* SPI */ spi_dev *spi_eng_dev; /* Configuration */ ad77681_power_mode power_mode; ad77681_mclk_div mclk_div; ad77681_conv_mode conv_mode; ad77681_conv_diag_mux diag_mux_sel; bool conv_diag_sel; ad77681_conv_len conv_len; ad77681_crc_sel crc_sel; uint8_t status_bit; } ad77681_dev; typedef struct { /* SPI */ spi_init_param *spi_eng_dev_init; /* Configuration */ ad77681_power_mode power_mode; ad77681_mclk_div mclk_div; ad77681_conv_mode conv_mode; ad77681_conv_diag_mux diag_mux_sel; bool conv_diag_sel; ad77681_conv_len conv_len; ad77681_crc_sel crc_sel; uint8_t status_bit; } ad77681_init_param; |