Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Next revisionBoth sides next revision
resources:eval:user-guides:ad7616-sdz [12 Dec 2022 12:48] Stanca-Florina Popresources:eval:user-guides:ad7616-sdz [10 Aug 2023 14:33] – [PL Interrupts] Stanca-Florina Pop
Line 75: Line 75:
  
 <code c> <code c>
-$ make SI_OR_PI=0+$ make SER_PAR_N=1
 </code> </code>
  
Line 81: Line 81:
  
 <code c> <code c>
-$ make SI_OR_PI=1+$ make SER_PAR_N=0
 </code> </code>
  
 <note important>Because of the **SDP-I-FMC** the level of the **VADJ** in the carrier board needs to be set to **3.3V**.</note> <note important>Because of the **SDP-I-FMC** the level of the **VADJ** in the carrier board needs to be set to **3.3V**.</note>
  
-=== PL Interrupts ===+==== CPU/Memory interconnects addresses ==== 
 + 
 +^ Instance             ^ Address    ^ 
 +|axi_ad7616_dma        | 0x44a30000 | 
 +|ad7616_pwm_gen        | 0x44b00000 | 
 +|spi_ad7616_axi_regmap | 0x44a00000 | 
 +|axi_ad7616            | 0x44a80000 | 
 + 
 +Note:  
 +  *  spi_ad7616 is instantiated only for SER_PAR_N=1  
 +  *  axi_ad7616 is instantiated only for SER_PAR_N=0 
 + 
 +==== PL Interrupts ====
  
 ^ Instance              ^ HDL interrupt ^ Linux PsU interrupt  ^ ^ Instance              ^ HDL interrupt ^ Linux PsU interrupt  ^
Line 107: Line 119:
  
 Note:  Note: 
-  *  axi_ad7616 is instantiated only for SI_OR_PI=1  +  *  spi_ad7616 is instantiated only for SER_PAR_N=1  
-  *  spi_ad7616 is instantiated only for SI_OR_PI=0+  *  axi_ad7616 is instantiated only for SER_PAR_N=0
  
  
-=== GPIO signals ===+==== GPIO signals ====
  
 Ps7 EMIO offset = 54 Ps7 EMIO offset = 54
resources/eval/user-guides/ad7616-sdz.txt · Last modified: 06 Dec 2023 11:11 by Esteban Blanc