This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:ad7403 [08 Oct 2014 12:55] – [User Notes] Aidan Frost | resources:eval:user-guides:ad7403 [30 Oct 2015 20:14] – [Downloads] Tom MacLeod | ||
---|---|---|---|
Line 18: | Line 18: | ||
<WRAP download> | <WRAP download> | ||
- | * http://www.analog.com/ | + | * http://download.analog.com/ |
- | * This link provides a download of the .zip file. Simply extract the .zip and launch AD7403.slx. This will launch [[mw> | + | * This link provides a download of the .zip file. Simply extract the .zip, run InstallMe.m, |
</ | </ | ||
====== User Notes ====== | ====== User Notes ====== | ||
- | To use the AD7403 model, ensure all the above packages are installed and download the zip file [[http://www.analog.com/ | + | To use the AD7403 model, ensure all the above packages are installed and download the zip file [[http://download.analog.com/ |
+ | |||
+ | In order to set up the paths, first navigate to the extracted directory and run | ||
+ | < | ||
+ | |||
+ | This is necessary for every new session of MATLAB. | ||
+ | |||
+ | Next, navigate to the AD7403 directory | ||
On opening Simulink, the following block diagram will appear. | On opening Simulink, the following block diagram will appear. |