Wiki

This version is outdated by a newer approved version.DiffThis version (16 Dec 2020 13:30) was approved by sergiu arpadi.

This is an old revision of the document!


AD469X HDL Reference Design

Overview

The AD469X HDL reference design provides all the interfaces that are necessary to interact with the devices on the AD469X eval board.

The design has a SPI Engine instance to control and acquire data from the AD4696 16-bit precisions ADC, providing support to capture continuous samples at maximum sampling rate. Currently the design supports the Zedboard.

Used devices

Supported FPGA carrier

HDL Design Description

The design is built upon ADI's generic HDL reference design framework. In the ADI Reference Designs HDL User Guide can be found an in-depth presentation and instructions about the HDL design framework in general.

The reference design uses the standard SPI Engine Framework to interface the AD4696 ADC in single SDO Mode. The SPI offload module, which can be used to capture continuous data stream at maximum data rate, is triggered by the BUSY signal of the device.

In order to build the HDL design the user has to go through the following steps:

  1. Confirm that you have the right tools (see Release notes)
  2. Clone the HDL GitHub repository (see https://wiki.analog.com/resources/fpga/docs/git)

No-OS Driver Description

Functions Declarations

Function Description
int32_t ad469x_spi_reg_read(struct ad469x_dev *dev,
			    uint16_t reg_addr,
			    uint8_t *reg_data);
Read device register.
int32_t ad469x_spi_reg_write(struct ad469x_dev *dev,
			     uint16_t reg_addr,
			     uint8_t reg_data);
Write device register
int32_t ad469x_spi_read_mask(struct ad469x_dev *dev,
			     uint16_t reg_addr,
			     uint8_t mask,
			     uint8_t *data);
Read from device using a mask
int32_t ad469x_spi_write_mask(struct ad469x_dev *dev,
			      uint16_t reg_addr,
			      uint8_t mask,
			      uint8_t data);
Write to device using a mask
int32_t ad469x_read_data(struct ad469x_dev *dev,
			 uint8_t channel,
			 uint32_t *buf,
			 uint16_t samples);
Read data from device
int32_t ad469x_seq_read_data(struct ad469x_dev *dev,
			     uint32_t *buf,
			     uint16_t samples);
Read from device when converter has the channel sequencer activated
int32_t ad469x_set_channel_sequence(struct ad469x_dev *dev,
				    enum ad469x_channel_sequencing seq);
Set channel sequence
int32_t ad469x_std_sequence_ch(struct ad469x_dev *dev,
			       uint16_t ch_mask);
Configure standard sequencer enabled channels
int32_t ad469x_adv_sequence_set_num_slots(struct ad469x_dev *dev,
						   uint8_t num_slots);
Configure advanced sequencer number of slots
int32_t ad469x_adv_sequence_set_slot(struct ad469x_dev *dev,
				     uint8_t slot,
				     uint8_t channel);
Advanced sequencer, assign channel to a slot
int32_t ad469x_sequence_enable_temp(struct ad469x_dev *dev);
Enable temperature read at the end of the sequence, for standard and advance sequencer
int32_t ad469x_sequence_disable_temp(struct ad469x_dev *dev);
Disable temperature read at the end of the sequence, for standard and advance sequencer
int32_t ad469x_adv_seq_osr(struct ad469x_dev *dev, uint16_t ch,
			   enum ad469x_osr_ratios ratio);
Configure over sampling ratio in advanced sequencer mode
int32_t ad469x_std_seq_osr(struct ad469x_dev *dev,
			   enum ad469x_osr_ratios ratio);
Configure over sampling ratio in standard sequencer mode
int32_t ad469x_enter_conversion_mode(struct ad469x_dev *dev);
Enter conversion mode
int32_t ad469x_exit_conversion_mode(struct ad469x_dev *dev);
Exit conversion mode
int32_t ad469x_init(struct ad469x_dev **device,
		    struct ad469x_init_param *init_param);
Initialize the device
int32_t ad469x_remove(struct ad469x_dev *dev);
Remove the device and release resources

Types Declarations

/**
 * @enum ad469x_channel_sequencing
 * @brief Channel sequencing modes
 */
enum ad469x_channel_sequencing {
	/** Single cycle read */
	AD469x_single_cycle,
	/** Two cycle read */
	AD469x_two_cycle,
	/** Sequence trough channels, standard mode */
	AD469x_standard_seq,
	/** Sequence trough channels, advanced mode */
	AD469x_advanced_seq,
};
 
/**
  * @enum ad469x_busy_gp_sel
  * @brief Busy state, possible general purpose pin selections
  */
enum ad469x_busy_gp_sel {
	/** Busy on gp0 */
	AD469x_busy_gp0 = 0,
	/** Busy on gp3 */
	AD469x_busy_gp3 = 1,
};
 
/**
  * @enum ad469x_reg_access
  * @brief Register access modes
  */
enum ad469x_reg_access {
	AD469x_BYTE_ACCESS,
	AD469x_WORD_ACCESS,
};
 
/**
  * @enum ad469x_supported_dev_ids
  * @brief Supported devices
  */
enum ad469x_supported_dev_ids {
	ID_AD4695,
	ID_AD4696,
	ID_AD4697,
};
 
/**
  * @enum ad469x_osr_ratios
  * @brief Supported oversampling ratios
  */
enum ad469x_osr_ratios {
	AD469x_OSR_1,
	AD469x_OSR_4,
	AD469x_OSR_16,
	AD469x_OSR_64
};
 
/**
 * @struct ad469x_init_param
 * @brief  Structure containing the init parameters needed by the ad469x device
 */
struct ad469x_init_param {
	/* SPI */
	spi_init_param		*spi_init;
	/* SPI module offload init */
	struct spi_engine_offload_init_param *offload_init_param;
	/* PWM generator init structure */
	struct pwm_init_param	*trigger_pwm_init;
	/** RESET GPIO initialization structure. */
	struct gpio_init_param	*gpio_resetn;
	/* Clock gen for hdl design init structure */
	struct axi_clkgen_init	*clkgen_init;
	/* Clock generator rate */
	uint32_t		axi_clkgen_rate;
	/* Register access speed */
	uint32_t		reg_access_speed;
	/* Register data width */
	uint8_t		reg_data_width;
	/* Capture data width */
	uint8_t		capture_data_width;
	/* Device Settings */
	enum ad469x_supported_dev_ids dev_id;
	/** Invalidate the Data cache for the given address range */
	void (*dcache_invalidate_range)(uint32_t address, uint32_t bytes_count);
};
 
/**
 * @struct ad469x_dev
 * @brief  Structure representing an ad469x device
 */
struct ad469x_dev {
	/* SPI descriptor */
	spi_desc		*spi_desc;
	/* Clock gen for hdl design structure */
	struct axi_clkgen	*clkgen;
	/* Trigger conversion PWM generator descriptor */
	struct pwm_desc		*trigger_pwm_desc;
	/* SPI module offload init */
	struct spi_engine_offload_init_param *offload_init_param;
	/* Register access speed */
	uint32_t		reg_access_speed;
	/* Register data width */
	uint8_t		reg_data_width;
	/* Capture data width */
	uint8_t		capture_data_width;
	/* Device Settings */
	enum ad469x_supported_dev_ids dev_id;
	/** RESET GPIO handler. */
	struct gpio_desc	*gpio_resetn;
	/** Invalidate the Data cache for the given address range */
	void (*dcache_invalidate_range)(uint32_t address, uint32_t bytes_count);
	/** Current channel sequence */
	enum ad469x_channel_sequencing ch_sequence;
	/** OSR resolution corresponding to each channel, when advanced
	 * sequencer is selected. */
	enum ad469x_osr_ratios adv_seq_osr_resol[AD469x_CHANNEL_NO];
	/** Channel slots for advanced sequencer */
	uint8_t ch_slots[AD469x_SLOTS_NO];
	/** Temperature enabled for standard and advanced sequencer if set. */
	bool temp_enabled;
	/** Number of active channel slots, for advanced sequencer */
	uint8_t num_slots;
};

HDL Downloads

Software sources

resources/eval/user-guides/ad469x.1607595996.txt.gz · Last modified: 10 Dec 2020 11:26 by Cristian Pop