This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad4130-8:softwareprocedures:demo_modes [27 Jun 2022 11:48] – Adding link positions to demo mode Cian McNamara | resources:eval:user-guides:ad4130-8:softwareprocedures:demo_modes [21 Jul 2022 16:15] (current) – Added 4 wire RTD demo mode Cian McNamara | ||
---|---|---|---|
Line 44: | Line 44: | ||
==== Noise test Demo ==== | ==== Noise test Demo ==== | ||
- | * **Warning: | + | * **Warning: |
If you have not set up the EVAL-AD4130-8WARDZ and controller board previously please go to the [[resources: | If you have not set up the EVAL-AD4130-8WARDZ and controller board previously please go to the [[resources: | ||
Line 69: | Line 69: | ||
=== Reading Samples from the ADC === | === Reading Samples from the ADC === | ||
Find the waveforms resulting from the gathered samples in the Analysis tab. The waveform graph shows each successive sample of the ADC output (input referred). The indicators beside this graph show the channels converting. The navigation tools allow you to control the cursor, zooming, and panning. You can also display the conversions as voltages or codes. | Find the waveforms resulting from the gathered samples in the Analysis tab. The waveform graph shows each successive sample of the ADC output (input referred). The indicators beside this graph show the channels converting. The navigation tools allow you to control the cursor, zooming, and panning. You can also display the conversions as voltages or codes. | ||
+ | Below the graph are parameters, such as peak-to-peak noise and rms noise, in the Results section for the current batch of samples. If there are several enabled analog input channels, you can select each enabled channel and the conversions through the analyzed channel using the Results Tab. | ||
+ | To save the data into an Excel file, select the Export button from the Results Tab. A Save dialog box is displayed, prompting you to save the data to an appropriate folder location. | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ==== RTD Demo mode ==== | ||
+ | * **Warning: | ||
+ | |||
+ | If you have not set up the EVAL-AD4130-8WARDZ and controller board previously please go to the [[resources: | ||
+ | |||
+ | If you have not set up/ | ||
+ | |||
+ | < | ||
+ | |||
+ | ==== 4-wire RTD Demo mode ==== | ||
+ | {{ : | ||
+ | Links that need to be adjusted for 4-wire RTD demo mode. | ||
+ | ^ Link Numbers | ||
+ | | LK4 | Black | Uninserted | Disconnects the onboard reference from REFIN1 (+) | Right of J10| | ||
+ | | LK5 | Blue | Uninserted | ||
+ | | LK6 | White |Uninserted| Disconnects REFIN1 (-) from AVSS | Left of Switch S3| | ||
+ | | LK7 | Black |Uninserted| Disconnects the onboard reference from REFIN1 (+) | Right of J10| | ||
+ | | LK35 |Red| Inserted| Precision Reference 5.11k ohm Resistor Bypass| Right of J8| | ||
+ | | LK36 |Red| Inserted| Headroom Resistor Bypass| Right J8| | ||
+ | {{ : | ||
+ | |||
+ | - Double click the AD4130-8 Eval Board icon to open the AD4130-8 Eval Board view window. The demo wizard will be on the left, either as shown in the figure below (Label 1) or already expanded. Expand the wizard by clicking the arrow (Label 2). {{ : | ||
+ | - With the wizard expanded, select the RTD button (Label 3). | ||
+ | - In the Configuration Options tab (Label 4), select 4 Wire for Number of Wires, select your RTD type either PT100 or PT1000 and pick which AVDD voltage you have set on the board either 1.8V or 3.3V. This will configure the AD4130-8 registers to the optimum RTD setup. | ||
+ | - The settings required for the demo are displayed to be viewed prior to writing to the AD4130-8 (Label 5). Click apply (Label 6) to write these settings to the board. | ||
+ | - The summary is then displayed once the write is complete (Label 1). {{ : | ||
+ | - From here navigate to the chip view by double-clicking the AD4130-8 chip (Label 2). | ||
+ | - To make further changes to the configuration click on the dark blue block in the chip view (Label 1) or double click the memory map option (Label 2) | ||
+ | - To begin capturing data double click the Analysis button (Label 3). {{ : | ||
+ | - To gather samples, change the Samples Count (Label 1) to the number of samples required, then click the Run Once button (Label 2) to acquire the samples from the ADC. The image below shows an example of the main window after running a RTD demo mode.{{ : | ||
+ | - To display the waveform data in degrees Celsius pick DegC in y-axis units dropdown (Label 3) | ||
+ | - For more information on the Waveform window go to the software section [[: | ||
+ | === Reading Samples from the ADC === | ||
+ | The evaluation board is set up to use the external 2.044 V in the RTD demo mode(when AVDD is set to 3.3V in Configuration Options tab or it is 1.022V if 1.8V is selected) on-board reference (From the 5.11k ohm precision resistor). To read samples from the ADC, do the following: | ||
+ | - The value in the Refin1(+/ | ||
+ | * Information on the reference choice can be viewed in the [[resources: | ||
+ | - When selecting Run Once, a batch of samples is read when clicking the button; the batch size is set by the value in the Samples field. | ||
+ | - When selecting Run Continuous, the software performs a continuous capture from the ADC by clicking the Run Once button. Click the Stop Capture button again to stop capturing data. | ||
+ | - Use the navigation tools within each graph to control the cursor, zooming, and panning. | ||
+ | |||
+ | === Reading Samples from the ADC === | ||
+ | Find the waveforms resulting from the gathered samples in the Analysis tab. The waveform graph shows each successive sample of the ADC output (input referred). The indicators beside this graph show the channels converting. The navigation tools allow you to control the cursor, zooming, and panning. You can also display the conversions as temperature (degrees Celsius) or codes. | ||
Below the graph are parameters, such as peak-to-peak noise and rms noise, in the Results section for the current batch of samples. If there are several enabled analog input channels, you can select each enabled channel and the conversions through the analyzed channel using the Results Tab. | Below the graph are parameters, such as peak-to-peak noise and rms noise, in the Results section for the current batch of samples. If there are several enabled analog input channels, you can select each enabled channel and the conversions through the analyzed channel using the Results Tab. | ||
To save the data into an Excel file, select the Export button from the Results Tab. A Save dialog box is displayed, prompting you to save the data to an appropriate folder location. | To save the data into an Excel file, select the Export button from the Results Tab. A Save dialog box is displayed, prompting you to save the data to an appropriate folder location. | ||
[[resources: | [[resources: |