Link Numbers | Colour | Default Position | Description | Rough Board Location |
---|---|---|---|---|
LK1-3 | White | Inserted | Ties AVSS and DGND together | N/A |
LK4 | Black | A | External Reference voltage select: Pos A: REFIN + is connected to the external +2.5V reference. Pos B: REFIN + is connected to the external +1.8V reference (+1.8V reference not currently available on the board). | Right of J10 |
LK5 | Blue | Inserted | Noise Test. Channels AIN0 + AIN1 | Right of Thermocouple Connection (A2) |
LK6 | White | Inserted | REFIN(-) to AVSS | Left of Switch S3 |
LK7 | Black | A | External +2.5V Reference: Pos A: ADR391B Pos B: ADR3625B (The ADR3625B is not currently available on the board) | Right of J10 |
LK8 | Black | Uninserted | Connects AIN10 to R95. When used with LK9 you can use the AD4130-8 to measure it's own IOVDD current | Left of T_IOVDD |
LK9 | Black | Uninserted | Connects AIN11 to R95. When used with LK8 you can use the AD4130-8 to measure it's own IOVDD current | Left of T_IOVDD |
LK10 | Black | Uninserted | Connects AIN12 to R96. When used with LK11 you can use the AD4130-8 to measure it's own AVDD current | Left of Switch S1 |
LK11 | Black | Uninserted | Connects AIN13 to R96. When used with LK10 you can use the AD4130-8 to measure it's own AVDD current | Left of Switch S1 |
LK12 | White | Uninserted | Connects AVSS to -1.8V. LK1-3 must be removed before this jumper is inserted | Right of Switch S1 |
LK14 | Black | Uninserted | Connects REFIN(+) to AVDD | Below 3.5mm Jack Connection (A1) |
LK15 | Black | A | ADP150-3.3 Powered up: Pos A: LDO is on Pos B: LDO is off | Below Switch S1 |
LK16 | Black | A | ADP150-1.8 Powered up: Pos A: LDO is on Pos B: LDO is off | Below Switch S1 |
LK17 | Black | A | Arduino communication: Pos A: Standard Pos B: Alternative | Between Arduino Connectors |
LK18 | Black | A | Arduino communication: Pos A: Standard Pos B: Alternative | Between Arduino Connectors |
LK19 | Black | A | Arduino communication: Pos A: Standard Pos B: Alternative | Between Arduino Connectors |
LK20 | Black | A | Arduino communication: Pos A: Standard Pos B: Alternative | Between Arduino Connectors |
LK21 | Black | Uninserted | Connects the CLK pin to the INT pin | Below T_IOVDD |
LK22 | Red | Uninserted | Thermocouple - Cold Junction Resistor Bypass | Left of Thermocouple Connection (A2) |
LK23 | Blue | Uninserted | Short EXC+/PSW: Pos Inserted = 4 Wire Bridge | Left of Switch S3 |
LK24 | Blue | Uninserted | Short EXC+/PSW: Pos Inserted = 4 Wire Bridge | Left of Switch S3 |
LK25 | Blue | Uninserted | Short EXC+/REFIN+: Pos Inserted = 4 Wire Bridge | Left of Switch S3 |
LK26 | Blue | Uninserted | Allows the user to use an external excitation source | Left of Switch S3 |
LK27 | Black | B | REFIN(+) to connector: Pos A: To Connector J10 (BRIDGE) Pos B: To Connector J8 (RTD) | Bottom right of J10 |
LK28 | Black | B | REFIN(-) to connector: Pos A: To Connector J10 (BRIDGE) Pos B: To Connector J8 (RTD) | Bottom right of J10 |
LK29 | White | Inserted | Connects CLK pin to GND | Left of J2 |
LK30 | Black | Uninserted | Connects AIN11 to LA_ELECTORDE trace of the A1 connector | Below 3.5mm Jack Connection (A1) |
LK31 | Black | Uninserted | Connects AIN14 to RA_ELECTORDE trace of the A1 connector | Below 3.5mm Jack Connection (A1) |
LK32 | Black | Uninserted | Connects AIN15 to DRIVEN_ELECTORDE trace of the A1 connector | Below 3.5mm Jack Connection (A1) |
LK35 | Red | Uninserted | Precision Reference 5.11k ohm Resistor Bypass | Right of J8 |
LK36 | Red | Uninserted | Headroom Resistor Bypass | Right J8 |
LK37 | Red | Uninserted | Precision Sense 10k ohm Resistor Bypass | Right of J8 |
LK45 | Black | Uninserted | AVDD/IOVDD short | Bottom Right of Switch S2 |
T_AVDD | Black | A | AVDD Supply: Pos A: Directly to supply rail Pos B: Through R96 (LK10 and 11 must be inserted) which allows the AD4130-8 to measure it's own AVDD current consumption | Below Switch S2 |
T_IOVDD | Black | A | IOVDD Supply: Pos A: Directly to supply rail Pos B: Through R95 (LK8 and 9 must be inserted) which allows the AD4130-8 to measure it's own IOVDD current consumption | Below Switch S2 |
S1 | Switch | +3.3V | AVDD Voltage connection: Pos A: +3.3V from the LDO Pos B: +1.8V from the LDO Pos C: +1.8V from the LDO Pos D: External voltage from J7 terminal block | Top of the Board |
S2 | Switch | +3.3V | IOVDD Voltage connection: Pos A: +3.3V from the LDO Pos B: +1.8V from the LDO Pos C: +1.8V from the LDO Pos D: External voltage from J7 terminal block | Top of the board |
S3 | Switch | REF1+/- | REFIN+/- connection: Pos A: REFIN1+/- Pos B: REFIN2+/- (AIN14 and AIN15) Pos C: REFOUT and AVSS (Internal Reference needs to be enabled in the ADC Control register) | Middle of the board |
If you have not set up the EVAL-AD4130-8WARDZ and controller board previously please go to the Quick Start Guide
If you have not set up/installed the ACE plugin before please go to Install Guide
The evaluation board is set up to use the external 2.5 V on-board reference (ADR391). To read samples from the ADC, do the following:
Find the waveforms resulting from the gathered samples in the Analysis tab. The waveform graph shows each successive sample of the ADC output (input referred). The indicators beside this graph show the channels converting. The navigation tools allow you to control the cursor, zooming, and panning. You can also display the conversions as voltages or codes. Below the graph are parameters, such as peak-to-peak noise and rms noise, in the Results section for the current batch of samples. If there are several enabled analog input channels, you can select each enabled channel and the conversions through the analyzed channel using the Results Tab. To save the data into an Excel file, select the Export button from the Results Tab. A Save dialog box is displayed, prompting you to save the data to an appropriate folder location.
If you have not set up the EVAL-AD4130-8WARDZ and controller board previously please go to the Quick Start Guide
If you have not set up/installed the ACE plugin before please go to Install Guide
Links that need to be adjusted for 4-wire RTD demo mode.
Link Numbers | Colour | 4-Wire RTD Demo mode Position | Description | Rough Board Location |
---|---|---|---|---|
LK4 | Black | Uninserted | Disconnects the onboard reference from REFIN1 (+) | Right of J10 |
LK5 | Blue | Uninserted | Disconnects AIN0 from AIN1 | Right of Thermocouple Connection (A2) |
LK6 | White | Uninserted | Disconnects REFIN1 (-) from AVSS | Left of Switch S3 |
LK7 | Black | Uninserted | Disconnects the onboard reference from REFIN1 (+) | Right of J10 |
LK35 | Red | Inserted | Precision Reference 5.11k ohm Resistor Bypass | Right of J8 |
LK36 | Red | Inserted | Headroom Resistor Bypass | Right J8 |
The evaluation board is set up to use the external 2.044 V in the RTD demo mode(when AVDD is set to 3.3V in Configuration Options tab or it is 1.022V if 1.8V is selected) on-board reference (From the 5.11k ohm precision resistor). To read samples from the ADC, do the following:
Find the waveforms resulting from the gathered samples in the Analysis tab. The waveform graph shows each successive sample of the ADC output (input referred). The indicators beside this graph show the channels converting. The navigation tools allow you to control the cursor, zooming, and panning. You can also display the conversions as temperature (degrees Celsius) or codes. Below the graph are parameters, such as peak-to-peak noise and rms noise, in the Results section for the current batch of samples. If there are several enabled analog input channels, you can select each enabled channel and the conversions through the analyzed channel using the Results Tab. To save the data into an Excel file, select the Export button from the Results Tab. A Save dialog box is displayed, prompting you to save the data to an appropriate folder location.