Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-trxboost1-ebz [19 Jul 2016 20:25]
charlyelkhoury added capital C
resources:eval:user-guides:ad-trxboost1-ebz [08 Nov 2016 14:58] (current)
charlyelkhoury removed the reference to software
Line 1: Line 1:
 ====== AD-TRXBOOST1-EBZ User Guide ====== ====== AD-TRXBOOST1-EBZ User Guide ======
  
-The [[adi>​AD-TRXBOOST1-EBZ]] is an add on board for the [[adi>​AD-FMCOMMS2-EBZ|FMCOMMS2/​3/​4/​5]] boards which contain the [[adi>​AD9361]]. While the complete chip level design package can be found on the ADI product pages of this RF transceiver,​ information on the card, and how to use itthe design package that surrounds it, and the software which can make it work, can be found here.+The [[adi>​AD-TRXBOOST1-EBZ]] is an add on board for the [[adi>​AD-FMCOMMS2-EBZ|FMCOMMS2/​3/​4/​5]] boards which contain the [[adi>​AD9361]]. While the complete chip level design package can be found on the ADI product pages of this RF transceiver,​ information on the card, and how to use it and the design package that surrounds it, can be found here.
  
 The purpose of the AD-TRXBOOST1-EBZ is to add an pre-amp to the TX output and an LNA to the RX input of the AD9361. The purpose of the AD-TRXBOOST1-EBZ is to add an pre-amp to the TX output and an LNA to the RX input of the AD9361.
resources/eval/user-guides/ad-trxboost1-ebz.txt · Last modified: 08 Nov 2016 14:58 by charlyelkhoury