Wiki

This version is outdated by a newer approved version.DiffThis version (25 Mar 2016 18:24) was approved by Neil Wilson.The Previously approved version (25 Mar 2016 18:18) is available.Diff

This is an old revision of the document!


Introduction

The AD-TRXBOOST1-EBZ module is comprised of the ADL5610 which is an 18dB RF fixed gain block that can operate between 30MHz and 6 GHz with a low noise figure of 2.2dB, the ADL5521 which is a 20dB LNA that can operate between 400MHz and 4GHz with a low noise figure of 0.8dB, along with the ADP2370 switch regulator and two ADP7104 LDOs.

For additional information or to purchase the AD-TRXBOOST1-EBZ, visit: www.analog.com/AD-TRXBOOST1-EBZ

Features

  • Includes schematics, layout, BOM, Gerber files
  • Powered from single Keyed connector that matches the header on the FMCOMMS2/3/4 series.
  • Provides one channel TX and one channel RX boost.

ADL5610 Gain Block

  • 30MHz to 6 GHz
  • Fixed gain of 18.4dB
  • Noise figure: 2.2dB at 900MHz
  • OIP3: 38.8dBm at 900MHz
  • P1dB: 20.4dBm at 900MHz
  • Single 5V supply

ADL5521 LNA

  • 400MHz to 4GHz
  • Fixed gain of 20.8dB at 900MHz
  • Noise figure: 0.8dB at 900MHz
  • OIP3: 37.0dBm at 900MHz
  • P1dB: 21.8dBm at 900MHz
  • Single supply between 3V and 5V

Applications

  • Electronic test and measurement equipment
  • General-purpose software radios
  • Radar systems
  • Ultra wideband satellite receivers
  • Signals intelligence (SIGINT)
  • Point to point communication systems
  • DOCSIS 3.0 CMTS and HFC networks
  • Multiple input/multiple output (MIMO) radios
  • Automated test equipment

Navigation - AD-TRXBOOST1-EBZ

resources/eval/user-guides/ad-trxboost1-ebz/introduction.1458926675.txt.gz · Last modified: 25 Mar 2016 18:24 by Neil Wilson