Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-pzsdr2400tdd-eb [18 Apr 2016 16:18]
Neil.wilson
resources:eval:user-guides:ad-pzsdr2400tdd-eb [30 Jul 2019 21:44] (current)
Larry Changed discontinued Avnet part number and links
Line 1: Line 1:
 ====== AD-PZSDR2400TDD-EB User Guide ====== ====== AD-PZSDR2400TDD-EB User Guide ======
  
-The [[adi>​AD-PZSDR2400TDD-EB]] is affectionately dubbed the first 'RF personality card'​. ​ It plugs into the Avnet [[http://zedboard.org/product/picozed-sdr-som-development-kit|AES-PZSDRCC-FMC-G]] carrier card. 35mm U.FL coaxial cables connect the card to the Avnet [[http://zedboard.org/product/picozed-sdr-som|PicoZed SDR Z7035/AD9361 SOM]] providing access to the transmit and receive inputs of the [[adi>​AD9361]]. ​ Information on the card, how to use it, the design package that surrounds it, and the software which can make it work, can be found here.+The [[adi>​AD-PZSDR2400TDD-EB]] is affectionately dubbed the first 'RF personality card'​. ​ It plugs into the ADRV1CRR-FMC ​[[https://www.analog.com/en/design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​ADRV1CRR-FMC.html]] carrier card. 35mm U.FL coaxial cables connect the card to the ADRV9361-Z7035 ​[[https://www.analog.com/en/design-center/​evaluation-hardware-and-software/evaluation-boards-kits/​ADRV9361-Z7035.html#​eb-overview]] providing access to the transmit and receive inputs of the [[adi>​AD9361]]. ​ Information on the card, how to use it, the design package that surrounds it, and the software which can make it work, can be found here.
  
 The purpose of the [[adi>​AD-PZSDR2400TDD-EB]] is to provide the user with a tunable path to condition the transmit or receive signals of the [[adi>​AD9361]]. ​ Selection of TX or RX path is achieved by the 200MHz to 2.7GHz SPDT switch [[adi>​HMC546LP2]] controlled by the FPGA and accompanying software. ​ The transmit path consists of a 2.4GHz filter, half watt driver amplifier [[adi>​ADL5324]] and 2 watt power amplifier [[adi>​HMC921]]. ​ The receive path consists of the same 2.4GHz filter as well as a low loss LNA [[adi>​HMC669]]. The purpose of the [[adi>​AD-PZSDR2400TDD-EB]] is to provide the user with a tunable path to condition the transmit or receive signals of the [[adi>​AD9361]]. ​ Selection of TX or RX path is achieved by the 200MHz to 2.7GHz SPDT switch [[adi>​HMC546LP2]] controlled by the FPGA and accompanying software. ​ The transmit path consists of a 2.4GHz filter, half watt driver amplifier [[adi>​ADL5324]] and 2 watt power amplifier [[adi>​HMC921]]. ​ The receive path consists of the same 2.4GHz filter as well as a low loss LNA [[adi>​HMC669]].
resources/eval/user-guides/ad-pzsdr2400tdd-eb.txt · Last modified: 30 Jul 2019 21:44 by Larry