Wiki

This version (27 Feb 2024 03:55) was approved by Zuedmar Arceo.The Previously approved version (06 Feb 2024 07:36) is available.Diff

AD-PAARRAY3552R-SL Software User Guide


Downloads

The AD-PAARRAY3552R-SL Embedded and Application Software files are available here:

AD-PAARRAY3552R-SL Software Files


The installer contains the following:

  • Embedded Software: AD-PARRAY3552R-SLv1.0.0.hex
  • Application Software: PA Array Biasing Software v1.0.0.exe
  • Evaluation License Agreement (ELA) for both firmware and GUI.
  • Wiki User Guide Link


Embedded Software

The AD-PAARRAY3552R is accompanied by an open-source software stack and associated collaterals, enabling a complete experience from evaluation and prototyping all the way to production firmware and applications development.

The system's firmware is based on Analog Devices' open-source ADI's no-OS framework, which includes most of the tools required for embedded code development and debugging as well as libraries enabling host-side connectivity for system configuration and data transfer over UART.


Updating the Firmware

The most common way of programming the system is by dragging and dropping the provided .hex file to the DAPLINK drive. Using the drag-and-drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the easiest way to get started with the reference design.


Setting up the MAX32625PICO

To update the board's firmware, a new bootloader has to be flashed on the MAX32625PICO. Follow below procedure:

  1. Download the firmware image: MAX32625PICO Firmware
  2. Do not connect the MAX32625PICO from the PC and the AD-PAARRAY3552R-SL board.
  3. Plug the micro-USB cable only in the MAX32625PICO.
  4. Press the button on the MAX32625PICO and then plug the other end of the micro-USB cable into the PC. (Do not release the button until the MAINTENANCE drive is mounted).
  5. Release the button once the MAINTENANCE drive is mounted.
  6. Drag and drop (to the MAINTENANCE drive) the firmware image.
  7. After a few seconds, the MAINTENANCE drive will disappear and be replaced by a drive named DAPLINK. This indicates that the process is complete, and the MAX32625PICO can now be used to flash the firmware of the AD-PAARRAY3552R-SL board.


Programming the AD-PAARRAY3552R-SL

  1. Connect the MAX32625PICO to the AD-PAARRAY3552R-SL board using the 10-pin ribbon cable.
  2. Connect the 48 V power supply to the AD-PAARRAY3552R-SL. Make sure the board is powered up for the next steps.
  3. A DAPLINK drive should appear as mounted on the PC.
  4. Drag and drop the AD-PAARRAY3552R-SLv1.0.0.hex into the DAPLINK drive. After a few seconds, the drive will be remounted.
  5. Check the DAPLINK directory and make sure there is no FAIL.TXT file. In case there is, repeat the drag and drop step. Otherwise, the MAX32625PICO can now be disconnected from the AD-PAARRAY3552R-SL, since the firmware update is complete.

Application Software

The system also integrates a graphical user interface (GUI) that continuously monitors crucial parameters. This interface facilitates complete system control, enabling faster prototyping and development.


Figure 1. Graphical User Interface (GUI)


The application software requires additional dependencies that need to be installed on PC for the GUI to function properly. To acquire these dependencies, click the link below.

Visit this page to download the required dependencies:

.NET Framework 4.6.2 Runtime


System Requirements

  • Windows 10 OS or later
  • Microsoft .Net Framework 4.6.2 Download
  • 1920 by 1080 or greater screen resolution, recommended
  • Keyboard and mouse
  • Optional internet connectivity to access online resources


Installation Instructions

  1. Extract the contents of the zip file.
  2. Open the AD-PAARRAY3552R-SL-Rel1.0.0 executable file.
  3. Install the program to the computer.
  4. Once the installation is complete, navigate to the default directory (C:\Analog Devices\AD-PAARRAY3552R-SL-Rel1.0.0\).


Graphical User Interface Walkthrough

This section provides a description and functionality details of the PA Array GUI. Access the Windows application by opening the PA Array Biasing Software v1.0.0.exe in the directory where the files have been installed.


Home Page

The Home Page provides an overview of the AD-PAARRAY3552R-SL, showcasing the description of the actual hardware and relevant links to help users to get started.


Dashboard

The Dashboard is where the user interacts with the hardware. It displays various groups with distinct functions.


Historical Graph

The Historical Graph pane shows the real-time temperature monitoring.


Device Group

The Device Connection displays a list of connected devices to connect and configure.


Control Group

The Control Group presents the control options and live values. This is where users can configure and monitor board functions.


Logs Group

The Logs pane displays the run-time logs that occur during board monitoring/configuration.





Further Help

For questions and more information about this product, connect with us through the Analog Devices Engineer Zone.

Navigation -


resources/eval/user-guides/ad-paarray3552r-sl/software.txt · Last modified: 27 Feb 2024 03:55 by Zuedmar Arceo