Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:ad-paarray3552r-sl:hardware [12 Feb 2024 02:00] – General formatting and other minor edits Joyce Velascoresources:eval:user-guides:ad-paarray3552r-sl:hardware [12 Feb 2024 02:19] (current) – [Hardware Connections] Zuedmar Arceo
Line 257: Line 257:
     * Marker is at 2.4 GHz     * Marker is at 2.4 GHz
   - Don't turn on the signal generator yet.   - Don't turn on the signal generator yet.
-  - Cascade the two HMC8500 GaN power amplifiers as shown in Figure 7 below.{{ :resources:eval:user-guides:pa_array:tbd.png?200 |}}  +  - Cascade the two HMC8500 GaN power amplifiers. 
-  - Connect the RF input/output of the signal chain to the signal generator and spectrum analyzer, respectively.{{ :resources:eval:user-guides:pa_array:tbd.png?200 |}}+  - Connect the RF input/output of the signal chain to the signal generator and spectrum analyzer, respectively.
   - For safety measures, turn off the bench power supply.   - For safety measures, turn off the bench power supply.
   - Connect the GND pin of the two HMC8500 to the GND pin of the AD-PAARRAY3552R-SL board.   - Connect the GND pin of the two HMC8500 to the GND pin of the AD-PAARRAY3552R-SL board.
   - Connect the gate pins (VGG) of the two HMC8500 to the VGC2 and VGP2 pins of the AD-PAARRAY3552R-SL board, respectively.   - Connect the gate pins (VGG) of the two HMC8500 to the VGC2 and VGP2 pins of the AD-PAARRAY3552R-SL board, respectively.
-  - Connect the drain pins (VDD) of the two HMC8500 to the VDC2 and VDP2 pins of the AD-PAARRAY3552R-SL board, respectively. Refer to the figure below.{{ :resources:eval:user-guides:pa_array:tbd.png?200 |}}+  - Connect the drain pins (VDD) of the two HMC8500 to the VDC2 and VDP2 pins of the AD-PAARRAY3552R-SL board, respectively.
   - Set the power supply voltage to +28 V before turning it on.   - Set the power supply voltage to +28 V before turning it on.
   - Connect the micro-USB to USB cable to Port P5 of the AD-PAARRAY3552R-SL and the other end of the cable to the computer.   - Connect the micro-USB to USB cable to Port P5 of the AD-PAARRAY3552R-SL and the other end of the cable to the computer.
-  - Open the GUI Application. In the GUI Homepage, click the **Go** button under the "Device Monitoring and Control" as shown below.{{ :resources:eval:user-guides:pa_array:tbd.png?200 |}} +  - Open the GUI Application. In the GUI Homepage, click the **Go** button under the "Device Monitoring and Control"
-  - It will show the GUI dashboard. On the device connection, choose the correct Serial Port. Then, press "Connect".{{ :resources:eval:user-guides:pa_array:tbd.png?200 |}}+  - It will show the GUI dashboard. On the device connection, choose the correct Serial Port. Then, press "Connect".
 \\ \\
 </WRAP> </WRAP>
resources/eval/user-guides/ad-paarray3552r-sl/hardware.txt · Last modified: 12 Feb 2024 02:19 by Zuedmar Arceo