Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-fxtof1-ebz [01 Jul 2021 23:42]
Andrei Cozma [Introduction]
resources:eval:user-guides:ad-fxtof1-ebz [21 Jul 2021 10:48] (current)
Andrei Cozma
Line 54: Line 54:
 <WRAP center round important 100%> <WRAP center round important 100%>
 Some of the AD-FXTOF1-EBZ kits are missing the correct 15 pins cable to connect to Raspberry Pi or the Nvidia platforms. If in your box there is only one 15 pins cable having the contacts on the same side, please get a new cable with contacts on opposite sides (e.g. [[https://​www.digikey.com/​en/​products/​detail/​w%C3%BCrth-elektronik/​686715152001/​4573357| 15 pins cable, contacts on opposite sides]]) Some of the AD-FXTOF1-EBZ kits are missing the correct 15 pins cable to connect to Raspberry Pi or the Nvidia platforms. If in your box there is only one 15 pins cable having the contacts on the same side, please get a new cable with contacts on opposite sides (e.g. [[https://​www.digikey.com/​en/​products/​detail/​w%C3%BCrth-elektronik/​686715152001/​4573357| 15 pins cable, contacts on opposite sides]])
 +
 +With the Raspberry Pi or the Nvidia platforms the 15 pins cable with contacts on opposite sides must be used for correct system operation. ​
 </​WRAP>​ </​WRAP>​
  
resources/eval/user-guides/ad-fxtof1-ebz.txt · Last modified: 21 Jul 2021 10:48 by Andrei Cozma