This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-fxtof1-ebz:ug_xavier_nx [17 Dec 2021 12:56] – Add point cloud description Septimiu Vana | resources:eval:user-guides:ad-fxtof1-ebz:ug_xavier_nx [21 Jan 2022 13:29] (current) – [Power on sequence] Andrei Cozma | ||
---|---|---|---|
Line 25: | Line 25: | ||
* Connect the HDMI cable from the monitor to the Jetson HDMI connector | * Connect the HDMI cable from the monitor to the Jetson HDMI connector | ||
* Connect the 25 pins flex cable between the camera and the interposer | * Connect the 25 pins flex cable between the camera and the interposer | ||
- | * Connect the 15 pons camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the interposer. Make sure to use the cable with contacts on opposite sides. | + | * Connect the 15 pons camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the interposer. |
+ | <WRAP center round important 100%> | ||
+ | Some of the AD-FXTOF1-EBZ kits are missing the correct 15 pins cable to connect to Raspberry Pi or the Nvidia platforms. If in your box there is only one 15 pins cable having the contacts on the same side, please get a new cable with contacts on opposite sides (e.g. [[https:// | ||
+ | </ | ||
* Connect a USB mouse and keyboard to the Xavier NX | * Connect a USB mouse and keyboard to the Xavier NX | ||
* Connect the power supply to the interposer | * Connect the power supply to the interposer |