This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fxtof1-ebz:ug_xavier_nx [19 Apr 2021 10:44] – Add fxtof1 demo image Septimiu Vana | resources:eval:user-guides:ad-fxtof1-ebz:ug_xavier_nx [16 Sep 2021 15:24] – [Prepare SD card] Septimiu Vana | ||
---|---|---|---|
Line 12: | Line 12: | ||
==== Prepare SD card ==== | ==== Prepare SD card ==== | ||
- | * Follow steps presented | + | * Download and flash on a SD card the latest image provided from the following link: [[repo> |
* Download L4T BSP [[https:// | * Download L4T BSP [[https:// | ||
* Extract kernel_src from BSP package | * Extract kernel_src from BSP package | ||
Line 24: | Line 24: | ||
* Plug the SD card into the Nvidia Xavier NX SD card slot | * Plug the SD card into the Nvidia Xavier NX SD card slot | ||
* Connect the HDMI cable from the monitor to the Jetson HDMI connector | * Connect the HDMI cable from the monitor to the Jetson HDMI connector | ||
- | * Connect the molex cable between the camera and the interposer | + | * Connect the 25 pins flex cable between the camera and the interposer |
- | * Connect the camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the interposer | + | * Connect the 15 pons camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the interposer. Make sure to use the cable with contacts on opposite sides. |
* Connect a USB mouse and keyboard to the Xavier NX | * Connect a USB mouse and keyboard to the Xavier NX | ||
* Connect the power supply to the interposer | * Connect the power supply to the interposer |