Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
Last revision Both sides next revision
resources:eval:user-guides:ad-fxtof1-ebz:ug_xavier_nx [19 Apr 2021 10:42]
Septimiu Vana Created fxtof1 user guide for xavier nx
resources:eval:user-guides:ad-fxtof1-ebz:ug_xavier_nx [21 Jul 2021 10:50]
Andrei Cozma [Power on sequence]
Line 24: Line 24:
   * Plug the SD card into the Nvidia Xavier NX SD card slot   * Plug the SD card into the Nvidia Xavier NX SD card slot
   * Connect the HDMI cable from the monitor to the Jetson HDMI connector   * Connect the HDMI cable from the monitor to the Jetson HDMI connector
-  * Connect the molex cable between the camera and the interposer +  * Connect the 25 pins flex cable between the camera and the interposer 
-  * Connect the camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the interposer+  * Connect the 15 pons camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the interposer. Make sure to use the cable with contacts on opposite sides.
   * Connect a USB mouse and keyboard to the Xavier NX   * Connect a USB mouse and keyboard to the Xavier NX
   * Connect the power supply to the interposer   * Connect the power supply to the interposer
Line 46: Line 46:
  
 [[https://​github.com/​analogdevicesinc/​aditof_sdk/​tree/​master/​examples/​aditof-demo | This example]] demonstrates how to capture data from the TOF system on the Nvidia Xavier NX and display it using OpenCV. ​ [[https://​github.com/​analogdevicesinc/​aditof_sdk/​tree/​master/​examples/​aditof-demo | This example]] demonstrates how to capture data from the TOF system on the Nvidia Xavier NX and display it using OpenCV. ​
 +
 +{{:​resources:​eval:​user-guides:​ad-96tof1-ebz:​aditof_demo.png|}}
  
 {{navigation AD-FXTOF1-EBZ#​none#​.:​|Overview#​none#​}} {{navigation AD-FXTOF1-EBZ#​none#​.:​|Overview#​none#​}}
  
resources/eval/user-guides/ad-fxtof1-ebz/ug_xavier_nx.txt · Last modified: 16 Sep 2021 15:24 by Septimiu Vana