Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:ad-fxtof1-ebz:ug_rpi [17 Jan 2022 12:50] – [Power on sequence] Andrei Cozmaresources:eval:user-guides:ad-fxtof1-ebz:ug_rpi [21 Jan 2022 13:27] (current) – [Power on sequence] Andrei Cozma
Line 18: Line 18:
   * Connect the HDMI cable from the monitor to the Raspberry Pi HDMI connector   * Connect the HDMI cable from the monitor to the Raspberry Pi HDMI connector
   * Connect the 25 pins flex cable between the camera and the interposer   * Connect the 25 pins flex cable between the camera and the interposer
-  * Connect the 15 pins camera cable between the RPi and the P1 connector of the interposer. **Make sure to use the cable with contacts on opposite sides.**+  * Connect the 15 pins camera cable between the RPi and the P1 connector of the interposer. **Make sure to use the cable with contacts on opposite sides.**  
 +<WRAP center round important 100%> 
 +Some of the AD-FXTOF1-EBZ kits are missing the correct 15 pins cable to connect to Raspberry Pi or the Nvidia platforms. If in your box there is only one 15 pins cable having the contacts on the same side, please get a new cable with contacts on opposite sides (e.g. [[https://www.digikey.com/en/products/detail/w%C3%BCrth-elektronik/686715152001/4573357| 15 pins cable, contacts on opposite sides]]) 
 +</WRAP>
   * Connect the interposer to the power supply   * Connect the interposer to the power supply
   * Connect the RPi to the power supply   * Connect the RPi to the power supply
resources/eval/user-guides/ad-fxtof1-ebz/ug_rpi.txt · Last modified: 21 Jan 2022 13:27 by Andrei Cozma