Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
Next revision Both sides next revision
resources:eval:user-guides:ad-fxtof1-ebz:ug_jetson [14 Apr 2021 14:08]
Septimiu Vana Created fxtof1 user guide for jetson
resources:eval:user-guides:ad-fxtof1-ebz:ug_jetson [16 Sep 2021 15:23]
Septimiu Vana [Prepare SD card]
Line 12: Line 12:
  
 ==== Prepare SD card ==== ==== Prepare SD card ====
-  * Follow steps presented ​on [[https://​developer.nvidia.com/​embedded/​learn/​get-started-jetson-nano-devkit#​write|Nvidia Website]] for creating Jetson Nano SD card+  * Download and flash on a SD card the latest image provided from the following link: [[repo>​aditof_sdk#​ad-fxtof1-ebz]]
   * Download L4T BSP [[https://​developer.nvidia.com/​embedded/​linux-tegra|L4T BSP]] package (Tested release R32.3.1)   * Download L4T BSP [[https://​developer.nvidia.com/​embedded/​linux-tegra|L4T BSP]] package (Tested release R32.3.1)
   * Extract kernel_src from BSP package   * Extract kernel_src from BSP package
Line 24: Line 24:
   * Plug the SD card into the Nvidia Jetson SD card slot   * Plug the SD card into the Nvidia Jetson SD card slot
   * Connect the HDMI cable from the monitor to the Jetson HDMI connector   * Connect the HDMI cable from the monitor to the Jetson HDMI connector
-  * Connect the molex cable between the camera and the interposer +  * Connect the 25 pins flex cable between the camera and the interposer 
-  * Connect the camera cable between the Jetson Nano and the P1 connector of the interposer+  * Connect the 15 pins camera cable between the Jetson Nano and the P1 connector of the interposer. Make sure to use the cable with contacts on opposite sides.
   * Connect a USB mouse and keyboard to the Jetson   * Connect a USB mouse and keyboard to the Jetson
   * Connect the interposer to the power supply   * Connect the interposer to the power supply
resources/eval/user-guides/ad-fxtof1-ebz/ug_jetson.txt · Last modified: 02 Nov 2021 09:15 by Septimiu Vana