Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-freqcvt1-ebz:testing [01 Mar 2016 23:07]
Tim Harder
resources:eval:user-guides:ad-freqcvt1-ebz:testing [02 Mar 2016 21:05]
Tim Harder add monitor, keyboard, and mouse info
Line 29: Line 29:
 ===== Required hardware ===== ===== Required hardware =====
  
-  * 1 ZC706 carrier board+  * 1 ZC706 carrier board and power supply 
 +  * 1 keyboard/​mouse 
 +  * 1 HDMI monitor
   * 1 SD test card   * 1 SD test card
   * 1 AD-FMCOMMS3-EBZ board   * 1 AD-FMCOMMS3-EBZ board
Line 41: Line 43:
 The FREQCVT1 testing should be done using the following steps: The FREQCVT1 testing should be done using the following steps:
  
-  - Make sure the ZC706 plugged in with the testing SD card inserted.+  - Make sure the ZC706 is plugged in with the testing SD card inserted ​and the HDMI monitor and keyboard/​mouse are properly attached to the system and powered on.
   - The FREQCVT1 board should be mounted on the TX2A/RX2A jacks of the AD-FMCOMMS3-EBZ board and the power cable and signal cables connected as seen in the image below. {{ :​resources:​eval:​user-guides:​ad-freqcvt1-ebz:​freqcvt1-testing-cables.jpg }}   - The FREQCVT1 board should be mounted on the TX2A/RX2A jacks of the AD-FMCOMMS3-EBZ board and the power cable and signal cables connected as seen in the image below. {{ :​resources:​eval:​user-guides:​ad-freqcvt1-ebz:​freqcvt1-testing-cables.jpg }}
   - Connect the RX_IN and TX_OUT jacks on the FREQCVT1 board with the SMA loopback cable.   - Connect the RX_IN and TX_OUT jacks on the FREQCVT1 board with the SMA loopback cable.
resources/eval/user-guides/ad-freqcvt1-ebz/testing.txt · Last modified: 02 Mar 2016 21:05 by Tim Harder