Wiki

This version (09 Feb 2021 18:43) was approved by Istvan Csomortani.

HDL support for AD-FREQCVT1-EBZ board

The AD-FREQCVT1-EBZ board can be configured through an SPI interface, using the provided 12-pin ribbon cable. Care should be taken to connect the cable to the PMOD connector the same way on carrier and board side too.

The FMCOMMS2/3 HDL design fully supports the AD-FREQCVT1-EBZ board by enabling the second SPI interface of the Processing System 7 IP core, in this way providing full access for the software to configure and setup the frequency converter board.

Supported carriers

Carrier PMOD connector
ZC706 J58
ZC702 J63
Zed Board JA1

IO layout

Carrier PMOD connector pin SPI interface FPGA pin name
ZC706 PMOD1_0 CSN_TX AJ21
PMOD1_4 CSN_RX Y20
PMOD1_3 SCLK AB16
PMOD1_1 DATA AK21
ZC702 PMOD1_0 CSN_TX E15
PL_PJTAG_TDI CSN_RX V8
PMOD1_3 SCLK W5
PMOD1_1 DATA D15
Zed JA1 CSN_TX Y11
JA7 CSN_RX AB11
JA4 SCLK AA9
JA2 DATA AA11
resources/eval/user-guides/ad-freqcvt1-ebz/hdl.txt · Last modified: 07 Mar 2016 17:37 by Istvan Csomortani