This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-fmcomms6-ebz [03 Nov 2016 10:42] – [AD-FMCOMMS6-EBZ User Guide] change "a pass band flatness of +/- 1.0 dB" Lucian Sin | resources:eval:user-guides:ad-fmcomms6-ebz [03 Jan 2021 22:04] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD-FMCOMMS6-EBZ User Guide ====== | ====== AD-FMCOMMS6-EBZ User Guide ====== | ||
- | The [[http:// | + | The [[adi>en/ |
This is an I and Q demodulation approach to direct convert (also known as a homodyne or zero IF) receiver architecture. Direct conversion radios perform just one frequency translation compared to a super-heterodyne receiver that can perform several frequency translations. One frequency translation is advantageous because it: | This is an I and Q demodulation approach to direct convert (also known as a homodyne or zero IF) receiver architecture. Direct conversion radios perform just one frequency translation compared to a super-heterodyne receiver that can perform several frequency translations. One frequency translation is advantageous because it: |