Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:ad-fmcomms5-ebz [09 Jul 2019 00:46] – ↷ Links adapted because of a move operation Robin Getz | resources:eval:user-guides:ad-fmcomms5-ebz [12 Feb 2021 15:01] (current) – fix links Robin Getz |
---|
| |
The purpose of the AD-FMCOMMS5-EBZ is to provide a platform to which shows how to connect and synchronize (at the RF side) multiple AD9361s for [[wp>MIMO|SIMO / MISO / SU-MIMO / MU-MIMO]] applications. To help with algorithm array processing development, there are a variety of things that can be done, from purchasing complete solutions: | The purpose of the AD-FMCOMMS5-EBZ is to provide a platform to which shows how to connect and synchronize (at the RF side) multiple AD9361s for [[wp>MIMO|SIMO / MISO / SU-MIMO / MU-MIMO]] applications. To help with algorithm array processing development, there are a variety of things that can be done, from purchasing complete solutions: |
* [[xilinx>products/intellectual-property/EF-DI-MIMODEC-LTE.htm|MIMO receiver]] | * [[xilinx>products/intellectual-property/do-di-mimoenc-lte.html|MIMO receiver]] |
* [[xilinx>products/intellectual-property/DO-DI-MIMOENC-LTE.htm|MIMO transmitter]] | * [[xilinx>products/intellectual-property/ef-di-mimodec-lte.html|MIMO transmitter]] |
To creating your own with something like [[mw>products/phased-array/|Phased Array System Toolbox]]. | To creating your own with something like [[mw>products/phased-array/|Phased Array System Toolbox]]. |
| |
====== Presentations ====== | ====== Presentations ====== |
| |
* [[https://www.analog.com/en/education/education-library/webcasts/developing-multiple-input-multiple-output.html|Developing Multiple-Input Multiple-Output (MIMO) Systems with the AD9361]] As Software Defined Radio (SDR) and Multiple-Input Multiple-Output (MIMO) become more prevalent there is a need for more channel diversity. This webcast will detail how to use multiple AD9361 devices to create an NxN MIMO system, as well as explore the available tradeoffs in the design. The AD9361 is a fully integrated 2x2 MIMO transceiver. Its programmability and wideband capability make it ideal for a broad range of transceiver applications. | * [[adi>en/education/education-library/webcasts/developing-multiple-input-multiple-output.html|Developing Multiple-Input Multiple-Output (MIMO) Systems with the AD9361]] As Software Defined Radio (SDR) and Multiple-Input Multiple-Output (MIMO) become more prevalent there is a need for more channel diversity. This webcast will detail how to use multiple AD9361 devices to create an NxN MIMO system, as well as explore the available tradeoffs in the design. The AD9361 is a fully integrated 2x2 MIMO transceiver. Its programmability and wideband capability make it ideal for a broad range of transceiver applications. |
| |
===== Warning ===== | ===== Warning ===== |
| |
{{page>wiki/common#esd_warning&nofooter&noheader}} | {{page>wiki/common#esd_warning&nofooter&noheader}} |