Wiki

This version is outdated by a newer approved version.DiffThis version (30 Aug 2019 04:43) was approved by Travis Collins.The Previously approved version (08 Aug 2019 18:28) is available.Diff

This is an old revision of the document!


AD-FMCOMMS5-EBZ Hardware

Downloads

Rev-B

ERRATA:

The FMCOMMS5, REV B has a bug in it, that doesn't allow the ADF5355 to function properly. (Pin 5, AVDD is a floating node). It's a simple fix - short pin 5 (AVDD) with pin 4 (CE) to make a connection to VDD_EXT_LO_3P3.

AD-FMCOMMS5-EBZ Rev B ADF5355 rework

Rev-C

I/O Voltage

The AD-FMComms5 (AD9361) assumes a VDD_INTERFACE voltage between 1.71V and 2.625V (1.8 to 2.5 +/- 5%), so on your FPGA carrier board, you should ensure that VADJ is between these levels. Setting things to 3.3V will damage the part.

Phase Synchronization

Traces between baluns and SMAs are not phase-matched on REV-A and REV-B which can cause phase misalignment with the libad9361-iio ad9361_fmcomms5_phase_sync solution. This is corrected on REV-C. Therefore, phase alignment performance can vary over frequency. The RF switches on REV-A/B are also not designed to work above 900 MHz. Higher frequency switches are available on REV-C.

Below are some preliminary results using Release 2018-R1 with equal length but unmatched cables

Rev B

Rev C

resources/eval/user-guides/ad-fmcomms5-ebz/hardware.1567033345.txt.gz · Last modified: 29 Aug 2019 01:02 by Travis Collins