Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:ad-fmcomms4-ebz:hardware [24 Oct 2016 10:56]
Lucian Sin change link for Johanson Technology's Balun
resources:eval:user-guides:ad-fmcomms4-ebz:hardware [19 May 2021 16:03] (current)
Robin Getz split rev B and C
Line 5: Line 5:
  
 <WRAP round download 65%> <WRAP round download 65%>
-<WRAP info>​This is the latest ​and greatest Rev "​B" ​of this board. Note that the Baluns on the Rev B board (T101-T104) are either :+<WRAP info>Note that the Baluns on the Rev C board (T101-T104) are either : 
 +  * Johanson Technology'​s [[http://​www.johansontechnology.com/​datasheets/​baluns/​JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. ​This balun is rated for a operating frequency of 2400~2500 MHz and is connected to RXB Input and TXB Output. If you want to evaluate the part outside ​of this frequency range, use the other SMA. 
 +  * Mini Circuits [[http://​www.minicircuits.com/​pdfs/​TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for a operating frequency between 70 MHz and 6 GHz, and are connected to the RXA Input and TXB Output. 
 +</​WRAP>​  
 +  * {{:​resources:​eval:​user-guides:​ad-fmcomms4-ebz:​02-037516-01-c-1.pdf|Rev C Schematics}} 
 +  * {{:​resources:​eval:​user-guides:​ad-fmcomms4-ebz:​09-037516-01C.zip|Rev C Gerbers}} (This file is [[http://​www.7-zip.org/​7z.html|compressed]]) 
 +  * {{:​resources:​eval:​user-guides:​ad-fmcomms4-ebz:​05-037516-01-c.xls||Rev C BOM}} 
 +</​WRAP>​ 
 + 
 +<WRAP round download 65%> 
 +<WRAP info>Note that the Baluns on the Rev B board (T101-T104) are either :
   * Johanson Technology'​s [[http://​www.johansontechnology.com/​datasheets/​baluns/​JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[../​ad-fmcomms2-ebz/​hardware/​configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology'​s 2450BL15B050E balun.   * Johanson Technology'​s [[http://​www.johansontechnology.com/​datasheets/​baluns/​JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[../​ad-fmcomms2-ebz/​hardware/​configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology'​s 2450BL15B050E balun.
   * Mini Circuits [[http://​www.minicircuits.com/​pdfs/​TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for a operating frequency between 10 MHz and 6 GHz.   * Mini Circuits [[http://​www.minicircuits.com/​pdfs/​TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for a operating frequency between 10 MHz and 6 GHz.
- 
 </​WRAP> ​ </​WRAP> ​
   * {{:​resources:​eval:​user-guides:​ad-fmcomms4-ebz:​02_037516b_top.pdf|Rev B Schematics}}   * {{:​resources:​eval:​user-guides:​ad-fmcomms4-ebz:​02_037516b_top.pdf|Rev B Schematics}}
   * {{:​resources:​eval:​user-guides:​ad-fmcomms4-ebz:​08_037516b.7z|Rev B Gerbers}} (This file is [[http://​www.7-zip.org/​7z.html|compressed]])   * {{:​resources:​eval:​user-guides:​ad-fmcomms4-ebz:​08_037516b.7z|Rev B Gerbers}} (This file is [[http://​www.7-zip.org/​7z.html|compressed]])
   * {{:​resources:​eval:​user-guides:​ad-fmcomms4-ebz:​fmcomms4_bom.xls||Rev B BOM}}   * {{:​resources:​eval:​user-guides:​ad-fmcomms4-ebz:​fmcomms4_bom.xls||Rev B BOM}}
-  * + 
     * The Epson crystal used on this board, has the generic part number "​TSX-3225 40.0000MHZ"​ - however, the generic part number does not have the specifications needed to meet the AD9361 datasheet specs. ADI has worked with Epson to provide a tighter tolerance part, which can be ordered as the "​OUTD-2B-0166"​ or "​X1E000021036701"​ (either part number will work, depending on which system your Epson contact/​distributor has) which meets the requirements that the AD9361 demands.     * The Epson crystal used on this board, has the generic part number "​TSX-3225 40.0000MHZ"​ - however, the generic part number does not have the specifications needed to meet the AD9361 datasheet specs. ADI has worked with Epson to provide a tighter tolerance part, which can be ordered as the "​OUTD-2B-0166"​ or "​X1E000021036701"​ (either part number will work, depending on which system your Epson contact/​distributor has) which meets the requirements that the AD9361 demands.
 </​WRAP>​ </​WRAP>​
resources/eval/user-guides/ad-fmcomms4-ebz/hardware.1477299397.txt.gz · Last modified: 24 Oct 2016 10:56 by Lucian Sin