Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Next revisionBoth sides next revision
resources:eval:user-guides:ad-fmcomms4-ebz:hardware [29 Apr 2014 21:32] – [I/O Voltage] Robin Getzresources:eval:user-guides:ad-fmcomms4-ebz:hardware [19 May 2021 16:03] – split rev B and C Robin Getz
Line 5: Line 5:
  
 <WRAP round download 65%> <WRAP round download 65%>
-<WRAP info>This is the latest and greatest Rev "B" of this board. Note that the Baluns on the Rev board (T101-T104) are either : +<WRAP info>Note that the Baluns on the Rev board (T101-T104) are either : 
-  * Johanson Technology's [[http://www.johansontechnology.com/images/stories/ip/baluns/Balun_2450BL15B050.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[../ad-fmcomms2-ebz/hardware/configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology's 2450BL15B050E balun+  * Johanson Technology's [[http://www.johansontechnology.com/datasheets/baluns/JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz and is connected to RXB Input and TXB Output. If you want to evaluate the part outside of this frequency range, use the other SMA
-  * Mini Circuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for a operating frequency between 10 MHz and 6 GHz.+  * Mini Circuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for a operating frequency between 70 MHz and 6 GHz, and are connected to the RXA Input and TXB Output. 
 +</WRAP>  
 +  * {{:resources:eval:user-guides:ad-fmcomms4-ebz:02-037516-01-c-1.pdf|Rev C Schematics}} 
 +  * {{:resources:eval:user-guides:ad-fmcomms4-ebz:09-037516-01C.zip|Rev C Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) 
 +  * {{:resources:eval:user-guides:ad-fmcomms4-ebz:05-037516-01-c.xls||Rev C BOM}} 
 +</WRAP>
  
 +<WRAP round download 65%>
 +<WRAP info>Note that the Baluns on the Rev B board (T101-T104) are either :
 +  * Johanson Technology's [[http://www.johansontechnology.com/datasheets/baluns/JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[../ad-fmcomms2-ebz/hardware/configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology's 2450BL15B050E balun.
 +  * Mini Circuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]. They are rated for a operating frequency between 10 MHz and 6 GHz.
 </WRAP>  </WRAP> 
   * {{:resources:eval:user-guides:ad-fmcomms4-ebz:02_037516b_top.pdf|Rev B Schematics}}   * {{:resources:eval:user-guides:ad-fmcomms4-ebz:02_037516b_top.pdf|Rev B Schematics}}
   * {{:resources:eval:user-guides:ad-fmcomms4-ebz:08_037516b.7z|Rev B Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]])   * {{:resources:eval:user-guides:ad-fmcomms4-ebz:08_037516b.7z|Rev B Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]])
 +  * {{:resources:eval:user-guides:ad-fmcomms4-ebz:fmcomms4_bom.xls||Rev B BOM}} 
 + 
     * The Epson crystal used on this board, has the generic part number "TSX-3225 40.0000MHZ" - however, the generic part number does not have the specifications needed to meet the AD9361 datasheet specs. ADI has worked with Epson to provide a tighter tolerance part, which can be ordered as the "OUTD-2B-0166" or "X1E000021036701" (either part number will work, depending on which system your Epson contact/distributor has) which meets the requirements that the AD9361 demands.     * The Epson crystal used on this board, has the generic part number "TSX-3225 40.0000MHZ" - however, the generic part number does not have the specifications needed to meet the AD9361 datasheet specs. ADI has worked with Epson to provide a tighter tolerance part, which can be ordered as the "OUTD-2B-0166" or "X1E000021036701" (either part number will work, depending on which system your Epson contact/distributor has) which meets the requirements that the AD9361 demands.
 </WRAP> </WRAP>
- 
 ===== I/O Voltage ===== ===== I/O Voltage =====
  
Line 57: Line 66:
 {{:resources:eval:user-guides:ad-fmcomms2-ebz:fmcomms2c_layers.png?direct&600|}} {{:resources:eval:user-guides:ad-fmcomms2-ebz:fmcomms2c_layers.png?direct&600|}}
  
-{{navigation AD-FMCOMMS2-EBZ#quickstart|Quick Start Guides#.:|Overview#reference_hdl|Reference HDL Design}}+
resources/eval/user-guides/ad-fmcomms4-ebz/hardware.txt · Last modified: 14 Mar 2023 06:10 by Joyce Velasco