This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | Next revision Both sides next revision | ||
resources:eval:user-guides:ad-fmcomms4-ebz:hardware [24 Oct 2016 10:56] Lucian Sin change link for Johanson Technology's Balun |
resources:eval:user-guides:ad-fmcomms4-ebz:hardware [15 Oct 2019 14:51] Mihai Bancisor [Downloads] |
||
---|---|---|---|
Line 13: | Line 13: | ||
* {{:resources:eval:user-guides:ad-fmcomms4-ebz:08_037516b.7z|Rev B Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) | * {{:resources:eval:user-guides:ad-fmcomms4-ebz:08_037516b.7z|Rev B Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) | ||
* {{:resources:eval:user-guides:ad-fmcomms4-ebz:fmcomms4_bom.xls||Rev B BOM}} | * {{:resources:eval:user-guides:ad-fmcomms4-ebz:fmcomms4_bom.xls||Rev B BOM}} | ||
+ | * {{:resources:eval:user-guides:ad-fmcomms4-ebz:02-037516-01-c-1.pdf|Rev C Schematics}} | ||
+ | * {{:resources:eval:user-guides:ad-fmcomms4-ebz:09-037516-01C.zip|Rev C Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) | ||
+ | * {{:resources:eval:user-guides:ad-fmcomms4-ebz:05-037516-01-c.xls||Rev C BOM}} | ||
* | * | ||
* The Epson crystal used on this board, has the generic part number "TSX-3225 40.0000MHZ" - however, the generic part number does not have the specifications needed to meet the AD9361 datasheet specs. ADI has worked with Epson to provide a tighter tolerance part, which can be ordered as the "OUTD-2B-0166" or "X1E000021036701" (either part number will work, depending on which system your Epson contact/distributor has) which meets the requirements that the AD9361 demands. | * The Epson crystal used on this board, has the generic part number "TSX-3225 40.0000MHZ" - however, the generic part number does not have the specifications needed to meet the AD9361 datasheet specs. ADI has worked with Epson to provide a tighter tolerance part, which can be ordered as the "OUTD-2B-0166" or "X1E000021036701" (either part number will work, depending on which system your Epson contact/distributor has) which meets the requirements that the AD9361 demands. |