This is an old revision of the document!
Shell scripts are scripts written for the shell (dash, bash, or ash) of an operating system. To find out which shell, you are using, try something like:
This specifies any shell prompt running on the target
rgetz@pinky ~ $ which sh /usr/bin/sh rgetz@pinky ~ $ ls -l /usr/bin/sh lrwxrwxrwx 1 root root 9 2009-05-13 20:39 /usr/bin/sh -> /bin/bash
OR
rgetz@pinky ~ $ ps -p $$ PID TTY TIME CMD 1321 pts/0 00:00:00 bash
To check out these scripts, simply do something like:
This specifies any shell prompt running on the target
rgetz@pinky ~ $ git clone https://github.com/analogdevicesinc/linux_image_ADI-scripts.git
This should give you the most up to date scripts.
By default, the Linux setup provided by ADI will try to automatically get an IP address from the network using DHCP. To instead use a static IP instead, do the following:
This specifies any shell prompt running on the target
root@linaro-ubuntu-desktop:~# sudo adi_update_tools.sh root@linaro-ubuntu-desktop:~# sudo enable_static_ip.sh <IP address>
In more detail, first make sure the latest software is installed on the host so the enable_static_ip.sh script is available. Then it can be used to set a static IP address for a network interface (defaults to eth0). Note that the specified IP address should generally be an unused one on the same subnet the device is getting added to. As a warning, note that these scripts will overwrite /etc/network/interfaces so do not run them on devices where you have specifically customized the network configuration.
An interface can be specified as the second argument otherwise the script defaults to eth0, e.g. in order to use 192.168.0.2 for eth1 run the following:
This specifies any shell prompt running on the target
root@linaro-ubuntu-desktop:~# sudo enable_static_ip.sh 192.168.0.2 eth1
In order to revert back to acquiring IP addresses for all interfaces via DHCP use the following:
This specifies any shell prompt running on the target
root@linaro-ubuntu-desktop:~# sudo enable_dhcp.sh
#!/bin/sh # find the DAC for i in $(find /sys -name name) do if [ "`cat $i`" = "cf-ad9361-dds-core-lpc" ] ; then dac_path=$(echo $i | sed 's:/name$::') fi done #save the current settings init=`cat $dac_path/out_altvoltage0_TX1_I_F1_frequency` sampl=`cat $dac_path/out_altvoltage_TX1_I_F1_sampling_frequency` ny=`expr $sampl / 2` # Set DDSn_A freq_A(){ echo $1 > $dac_path/out_altvoltage0_TX1_I_F1_frequency echo $1 > $dac_path/out_altvoltage2_TX1_Q_F1_frequency echo $1 > $dac_path/out_altvoltage4_TX2_I_F1_frequency echo $1 > $dac_path/out_altvoltage6_TX2_Q_F1_frequency } # Set DDSn_B freq_B(){ echo $1 > $dac_path/out_altvoltage3_TX1_Q_F2_frequency echo $1 > $dac_path/out_altvoltage1_TX1_I_F2_frequency echo $1 > $dac_path/out_altvoltage7_TX2_Q_F2_frequency echo $1 > $dac_path/out_altvoltage5_TX2_I_F2_frequency } for i in `seq 1000000 1000000 $ny` do freq_A $i freq_B `expr $ny - $i` sleep 1 done freq_A $init freq_B $init
#!/bin/sh # buffer size, let's use 512 samples, or 1024 bytes buffer_size=1024 # find the DAC for i in $(find /sys -name name) do if [ "`cat $i`" = "cf-ad9361-dds-core-lpc" ] ; then dac_path=$(echo $i | sed 's:/name$::') fi done # Get the associated dev file dev=/dev/$(echo $dac_path | awk -F "/" '{print $NF}') if [ ! -c $dev ] ; then echo "Can't find device $dev" exit fi # set the buffer size echo $buffer_size > $dac_path/buffer/length # generate the random data, and give it to the DAC dd if=/dev/urandom of=$dev bs=$buffer_size count=1 #enable things echo 1 > $dac_path/buffer/enable #Wait 5 seconds sleep 5 #turn if off before we bring down everyone's WiFi echo 0 > $dac_path/buffer/enable
I don't like remembering what 1/32 is, so I just use . You just need to provide 'n'.
#!/bin/sh #check in the input if [ $1 -le -1 ] ; then echo "input out of range, (needs to be 0-15)" exit fi if [ $1 -ge 16 ] ; then echo "input out of range (needs to be 0-15)" exit fi # find the DAC for i in $(find /sys -name name 2>/dev/null) do if [ "`cat $i`" = "cf-ad9361-dds-core-lpc" ] ; then dac_path=$(echo $i | sed 's:/name$::') fi done echo $(echo "scale=6; 1 / ( 2 ^ $1 )" | bc) > $dac_path/out_altvoltage0_TX1_I_F1_scale echo $(echo "scale=6; 1 / ( 2 ^ $1 )" | bc) > $dac_path/out_altvoltage1_TX1_I_F2_scale echo $(echo "scale=6; 1 / ( 2 ^ $1 )" | bc) > $dac_path/out_altvoltage2_TX1_Q_F1_scale echo $(echo "scale=6; 1 / ( 2 ^ $1 )" | bc) > $dac_path/out_altvoltage3_TX1_Q_F2_scale echo $(echo "scale=6; 1 / ( 2 ^ $1 )" | bc) > $dac_path/out_altvoltage4_TX2_I_F1_scale echo $(echo "scale=6; 1 / ( 2 ^ $1 )" | bc) > $dac_path/out_altvoltage5_TX2_I_F2_scale echo $(echo "scale=6; 1 / ( 2 ^ $1 )" | bc) > $dac_path/out_altvoltage6_TX2_Q_F1_scale echo $(echo "scale=6; 1 / ( 2 ^ $1 )" | bc) > $dac_path/out_altvoltage7_TX2_Q_F2_scale echo -n "amplitude set to " cat $dac_path/out_altvoltage0_TX1_I_F1_scale
#!/bin/sh # find the TX LO generator for i in $(find /sys -name name) do if [ "`cat $i`" = "ad9361-phy" ] ; then tx_lo_path=$(echo $i | sed 's:/name$::') fi done if [ -z $tx_lo_path ] ; then echo "Can't find ad9361-phy" exit 1 fi start=$1 end=$2 inc=$3 pause=$4 if [ -z $start ] ; then start=100 fi if [ -z $end ] ; then end=6000 fi if [ -z $inc ] ; then inc=5 fi if [ -z $pause ] ; then pause=1 fi freq_tx() { echo $1 > $tx_lo_path/out_altvoltage1_TX_LO_frequency } for i in `seq $start $inc $end`; do echo $i freq_tx `expr $i \\* 1000000` sleep $pause done