This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcomms2-ebz:software:datafiles [18 Feb 2014 22:56] – [Data Verification] Di Pu | resources:eval:user-guides:ad-fmcomms2-ebz:software:datafiles [27 Jan 2021 22:20] (current) – use wp> interwiki links Robin Getz | ||
---|---|---|---|
Line 14: | Line 14: | ||
* DSP System Toolbox Version 8.5 | * DSP System Toolbox Version 8.5 | ||
</ | </ | ||
+ | |||
+ | ===== Data transfer ===== | ||
+ | |||
+ | Once files have been created by MATLAB/ | ||
+ | |||
===== QPSK ===== | ===== QPSK ===== | ||
Line 38: | Line 43: | ||
=== Data === | === Data === | ||
+ | <WRAP round info 65%> | ||
+ | Once the transmitted signals are in workspace, we use the following two lines to write them to a text file: | ||
+ | |||
+ | <code matlab> | ||
+ | newdata = [I1 Q1 I2 Q2]; | ||
+ | |||
+ | dlmwrite(' | ||
+ | </ | ||
+ | |||
+ | You open this text file and manually add the word " | ||
+ | | ||
+ | </ | ||
+ | |||
+ | |||
<WRAP round download 80%> | <WRAP round download 80%> | ||
You can download the generated data from below: | You can download the generated data from below: | ||
Line 58: | Line 77: | ||
=== Model === | === Model === | ||
- | The figure below shows a QPSK transmission model with the pulse shaping filters. Since pulse shaping filters are often distributed as a matched pair between transmitter and receiver, we use the filter shape of ‘Square root’(([[http:// | + | The figure below shows a QPSK transmission model with the pulse shaping filters. Since pulse shaping filters are often distributed as a matched pair between transmitter and receiver, we use the filter shape of ‘Square root’(([[wp>Root-raised-cosine_filter|Root-raised-cosine filter]])). |
{{QPSKwithfilter.png? | {{QPSKwithfilter.png? | ||
Line 98: | Line 117: | ||
{{iiosetting_new.png? | {{iiosetting_new.png? | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The DCXO setting can be different from board to board. You are suggested to find a proper setting using signal generator and spectrum analyzer in the lab. | ||
+ | </ | ||
Since there is no match filter on AD9361 receive path, the data obtained from AD9361 receiver side does not show the constellation of QPSK clearly. Therefore, by simply looking at the ADI IIO Oscilloscope, | Since there is no match filter on AD9361 receive path, the data obtained from AD9361 receiver side does not show the constellation of QPSK clearly. Therefore, by simply looking at the ADI IIO Oscilloscope, | ||
Line 120: | Line 143: | ||
You can download the receiver model from below: | You can download the receiver model from below: | ||
- | * {{qpsk_receiver_new.zip}} | + | * {{qpsk_receiver_new.zip}} |
+ | |||
+ | Make sure you load the mat data file in the workspace first. Otherwise, the model will not run. | ||
The data rate is defined in the parameter '' | The data rate is defined in the parameter '' | ||
</ | </ | ||
Line 182: | Line 208: | ||
===== MSK ===== | ===== MSK ===== | ||
- | MSK stands for minimum shift keying. It is one type of the continuous phase modulation (CPM) schemes (([[http:// | + | MSK stands for minimum shift keying. It is one type of the continuous phase modulation (CPM) schemes (([[wp>Minimum-shift_keying|Minimum-shift keying]])). In this section, we use "MSK Modulator Baseband" |
==== Model ==== | ==== Model ==== | ||
Line 240: | Line 266: | ||
The figure below shows a LTE example according to the specifications developed by the Third Generation Partnership Project (3GPP). It highlights only the downlink physical channel (PDSCH) processing. | The figure below shows a LTE example according to the specifications developed by the Third Generation Partnership Project (3GPP). It highlights only the downlink physical channel (PDSCH) processing. | ||
- | Since LTE is a sophisticated standard, you are encouraged to read the Help Document of this example and its related references to get more information (([[http:// | + | Since LTE is a sophisticated standard, you are encouraged to read the Help Document of this example and its related references to get more information (([[mw>help/ |
{{LTE.png? | {{LTE.png? |