Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-fmcomms2-ebz:software:baremetal [13 Aug 2018 16:34]
DragosB Remove unsupported platforms
resources:eval:user-guides:ad-fmcomms2-ebz:software:baremetal [13 Aug 2018 16:35]
DragosB Fix ad9361_rx_fastlock_load() description
Line 74: Line 74:
 |<code c>​int32_t ad9361_rx_fastlock_store(struct ad9361_rf_phy *phy, uint32_t profile)</​code>​|Stores RX fastlock profile. To create a profile tune the synthesizer (ad9361_set_rx_lo_freq()) and then call this function specifying the target profile number. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise.| |<code c>​int32_t ad9361_rx_fastlock_store(struct ad9361_rf_phy *phy, uint32_t profile)</​code>​|Stores RX fastlock profile. To create a profile tune the synthesizer (ad9361_set_rx_lo_freq()) and then call this function specifying the target profile number. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise.|
 |<code c>​int32_t ad9361_rx_fastlock_recall(struct ad9361_rf_phy *phy, uint32_t profile)</​code>​|Recalls specified RX fastlock profile. When in fastlock pin select mode (init_param->​rx_fastlock_pincontrol_enable),​ the function needs to be called before then the pin-control can be used. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise.| |<code c>​int32_t ad9361_rx_fastlock_recall(struct ad9361_rf_phy *phy, uint32_t profile)</​code>​|Recalls specified RX fastlock profile. When in fastlock pin select mode (init_param->​rx_fastlock_pincontrol_enable),​ the function needs to be called before then the pin-control can be used. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise.|
-|<code c>​ad9361_rx_fastlock_load</​code>​|Recalls specified RX fastlock profile. When in fastlock pin select mode (init_param->​rx_fastlock_pincontrol_enable),​ the function needs to be called before then the pin-control can be used. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the Fastlock profile program data (val0,​val1,​val2,​...,​val15). Returns 0 in case of success, negative error code otherwise.|+|<code c>int32_t ​ad9361_rx_fastlock_load(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values)</​code>​|Recalls specified RX fastlock profile. When in fastlock pin select mode (init_param->​rx_fastlock_pincontrol_enable),​ the function needs to be called before then the pin-control can be used. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the Fastlock profile program data (val0,​val1,​val2,​...,​val15). Returns 0 in case of success, negative error code otherwise.|
 |<code c>​int32_t ad9361_rx_fastlock_save(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values)</​code>​|Saves RX fastlock profile. In order to use more than 8 Profiles, an existing profile can be read back and stored by the user application. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the location for storing the profile data. Returns 0 in case of success, negative error code otherwise.| |<code c>​int32_t ad9361_rx_fastlock_save(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values)</​code>​|Saves RX fastlock profile. In order to use more than 8 Profiles, an existing profile can be read back and stored by the user application. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the location for storing the profile data. Returns 0 in case of success, negative error code otherwise.|
 |<code c>​int32_t ad9361_rx_lo_powerdown(struct ad9361_rf_phy *phy, uint8_t option)</​code>​|Powers down the RX Local Oscillator. Receives as parameters a structure that contains the AD9361 current state and the option (ON, OFF). Returns 0 in case of success, negative error code otherwise.| |<code c>​int32_t ad9361_rx_lo_powerdown(struct ad9361_rf_phy *phy, uint8_t option)</​code>​|Powers down the RX Local Oscillator. Receives as parameters a structure that contains the AD9361 current state and the option (ON, OFF). Returns 0 in case of success, negative error code otherwise.|
resources/eval/user-guides/ad-fmcomms2-ebz/software/baremetal.txt · Last modified: 13 Aug 2018 16:35 by DragosB