This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcomms2-ebz:software:baremetal:arradio_noos [19 Sep 2017 16:04] – [Running the no-OS software (2R2T)] rejeesh kutty | resources:eval:user-guides:ad-fmcomms2-ebz:software:baremetal:arradio_noos [19 Sep 2017 16:10] – rejeesh kutty | ||
---|---|---|---|
Line 232: | Line 232: | ||
</ | </ | ||
+ | <WRAP center round info 100%> | ||
The design supports both 2R2T mode (AD9361 only) and 1R1T mode (AD9361 and AD9364). The rest of the UART log will be different accordingly. | The design supports both 2R2T mode (AD9361 only) and 1R1T mode (AD9361 and AD9364). The rest of the UART log will be different accordingly. | ||
+ | </ | ||
===== Running the no-OS software (2R2T) ===== | ===== Running the no-OS software (2R2T) ===== | ||
Line 331: | Line 333: | ||
Done. | Done. | ||
</ | </ | ||
+ | |||
+ | ===== Switching between 2R2T & 1R1T mode(s) ===== | ||
+ | |||
+ | After the first run, the build remembers (until you do a clean) your mode of choice and subsequent builds (in case you modify the sources) assume this mode as default. As a precaution, always cross check the compiler flags mentioned above with your desired mode. | ||
+ | |||
+ | < | ||
+ | [some-dir]> | ||
+ | [some-dir]> | ||
+ | [some-dir]> | ||
+ | [some-dir]> | ||
+ | </ | ||
+ | |||