Wiki

This version is outdated by a newer approved version.DiffThis version (25 Jan 2021 13:44) was approved by Mihai Ionut Suciu.The Previously approved version (30 May 2019 17:45) is available.Diff

This is an old revision of the document!


AD936X Quick Start Guides

AD-FMCOMMS2/3/4/5-EBZ

The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the AD-FMCOMMS2/3/4/5-EBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.

Supported Carriers

The AD-FMCOMMS2/3/4/5-EBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:

Board FMCOMMS5 FMCOMMS2/3/4 Arradio
AC701
KC705
KCU105
VC707
ZC702
ZC706
ZCU102
Zed Board
MITX045
SoCKit

Supported Environments

The supported OS are:

Board HDL Linux Software No-OS Software
AC701
KC705
KCU105
VC707
ZC702
ZC706
ZCU102
Zed Board
MITX045

Hardware Setup

In most carriers, the AD-FMCOMMS2/3/4-EBZ board connects to the LPC connector (unless otherwise noted). The AD-FMCOMMS5-EBZ board is a dual FMC connector, and requires either FMC connectors (which can be either LPC + LPC). The carrier setup requires power, UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.

ZC702 + FMCOMMS2

Early versions of the ZC702 carriers need to work around AR# 51438, PG signal does not assert by default errata.

ZC706 + FMCOMMS2

SoCkit + ARRADIO

Jumper Configuration

CLOCKSEL0 CLOCKSEL1 BOOTSEL0 BOOTSEL1 BOOTSEL2
POS 2-3 2-3 2-3 2-3 1-2

JP2
1.8V or 2.5V

MSEL0 MSEL1 MSEL2 MSEL3 MSEL4 CODEC_SEL
POS 0 0 1 0 0 0

ADRV936X System-On-Module

The ADRV936X SOMs have three selectable switches. Two are used for selecting the boot source, and one for selecting the SD card source. The selection will be based on your carrier and how you want to boot the device.

For switch S3 and S4

BOOT Mode S3 S4
JTAG 0 0
QSPI 0 1
SD Card 1 1

For switch S1:

SD Card Source S1
Onboard 0
Carrier 1

For our standard evaluation system most users boot from the SD cards placed either on the SOM or carrier board. For the ADRV1CRR-BOB carrier or carriers without SD card slots be sure to set S1 to 0.

Networking

By default, all SD cards for the prototyping platform (not TES) are configured for DHCP networking over their Ethernet interfaces. If you want to change the networking interfaces to use static addresses, which is required for directly connected Ethernet cables without DHCP servers in the loop, a helper script is provided.

To update the IP address of the board you must be logged into the board over UART or JTAG or Ethernet.

From the development board or SOM itself run the following with the desired IP address:

enable_static_ip.sh <ip address> eth0

This will fix the IP address of the desired Ethernet adapter and prevent the onboard network manager from changing it.

resources/eval/user-guides/ad-fmcomms2-ebz/quickstart.1611578639.txt.gz · Last modified: 25 Jan 2021 13:43 by Mihai Ionut Suciu