Wiki

This version is outdated by a newer approved version.DiffThis version (26 Feb 2016 09:14) is a draft.
Approvals: 0/1
The Previously approved version (21 Aug 2015 17:16) is available.Diff

This is an old revision of the document!


AD-FMCOMMS2/3/4/5-EBZ Quick Start Guides

The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the AD-FMCOMMS2/3/4/5-EBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.

Supported Carriers

The AD-FMCOMMS2/3/4/5-EBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:

Board FMCOMMS5 FMCOMMS2/3/4 Arradio
AC701
KC705
VC707
ZC702
ZC706
Zed Board
MITX045
SoCKit

Supported Environments

The supported OS are:

Board HDL Linux Software No-OS Software
AC701
KC705
VC707
ZC702
ZC706
Zed Board

Hardware Setup

In most carriers, the AD-FMCOMMS2/3/4-EBZ board connects to the LPC connector (unless otherwise noted). The AD-FMCOMMS5-EBZ board is a dual FMC connector, and requires either FMC connectors (which can be either LPC + LPC). The carrier setup requires power, UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.

ZC702 + FMCOMMS2

Early versions of the ZC702 carriers need to work around AR# 51438, PG signal does not assert by default errata.

ZC706 + FMCOMMS2

SoCkit + ARRADIO

Jumper Configuration

CLOCKSEL0 CLOCKSEL1 BOOTSEL0 BOOTSEL1 BOOTSEL2
POS 2-3 2-3 2-3 2-3 1-2

JP2
1.8V or 2.5V

MSEL0 MSEL1 MSEL2 MSEL3 MSEL4 CODEC_SEL
POS 0 0 1 0 0 0

resources/eval/user-guides/ad-fmcomms2-ebz/quickstart.1456474450.txt.gz · Last modified: 26 Feb 2016 09:14 by Mihai Ionut Suciu