This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:user-guides:ad-fmcomms2-ebz:quickstart:zynq [04 Jun 2021 20:29] Robin Getz [AD-FMCOMMS2/3/4/5-EBZ Zynq and ZED Quick Start Guide] |
resources:eval:user-guides:ad-fmcomms2-ebz:quickstart:zynq [09 Jun 2021 12:11] Iulia Moldovan Add details to link |
||
---|---|---|---|
Line 19: | Line 19: | ||
===== Creating / Configuring the SD Card ===== | ===== Creating / Configuring the SD Card ===== | ||
- | [[resources/tools-software/linux-software/zynq_images|Create SD Image for Zynq/ZED Boards. (it is a single image for all boards)]] | + | Create the [[resources/tools-software/linux-software/zynq_images|SD Image]] for Zynq/ZED Boards. (it is a single image for all boards) |
{{page>wiki/common#esd_warning&nofooter&noheader}} | {{page>wiki/common#esd_warning&nofooter&noheader}} | ||
Line 29: | Line 29: | ||
- Get the [[xilinx>ZC706]] | - Get the [[xilinx>ZC706]] | ||
- {{http://www.xilinx.com/images/product-images/zc706-base-board.jpg}} | - {{http://www.xilinx.com/images/product-images/zc706-base-board.jpg}} | ||
- | - Build the HDL project and make the BOOT.BIN (see [[:resources:fpga:docs:build|this tutorial]]) | + | - Prepare the SD card with the proper Linux image (from [[:resources:tools-software:linux-software:zynq_images|here]] and pay attention to the Linux/Windows setup). |
- | - Build the devicetree (see [[:resources:tools-software:linux-build:generic:zynq|this tutorial]]) | + | |
- | - Prepare the SD card with the proper Linux image (see [[:resources:tools-software:linux-software:zynq_images|here]] and pay attention to the Linux/Windows setup), BOOT.BIN, and devicetree (you get the last ones from the previous steps) | + | |
- Insert the SD-CARD into the SD Card Interface Connector (J30) | - Insert the SD-CARD into the SD Card Interface Connector (J30) | ||
- Plug the AD-FMCOMMS2-EBZ into the LPC LPC Connector (J5) | - Plug the AD-FMCOMMS2-EBZ into the LPC LPC Connector (J5) | ||
Line 42: | Line 40: | ||
- Wait another ~30 seconds for the HDMI display device to start showing signs of life. | - Wait another ~30 seconds for the HDMI display device to start showing signs of life. | ||
- The follow the instructions for the type of demo that you want to do. | - The follow the instructions for the type of demo that you want to do. | ||
+ | |||
===== Booting the SD Card ===== | ===== Booting the SD Card ===== | ||
Line 59: | Line 58: | ||
- Set the Jumpers and Switches accordingly like shown on the picture. (click on the picture to enlarge) | - Set the Jumpers and Switches accordingly like shown on the picture. (click on the picture to enlarge) | ||
- {{:resources:eval:user-guides:ad-fmcomms2-ebz:quickstart:zed_sw.jpg?300|ZED Board prepared}} | - {{:resources:eval:user-guides:ad-fmcomms2-ebz:quickstart:zed_sw.jpg?300|ZED Board prepared}} | ||
- | - Build the HDL project and make the BOOT.BIN (see [[:resources:fpga:docs:build|this tutorial]]) | + | - Prepare the SD card with the proper Linux image (see [[:resources:tools-software:linux-software:zynq_images|here]] and pay attention to the Linux/Windows setup) |
- | - Build the devicetree (see [[:resources:tools-software:linux-build:generic:zynq|this tutorial]]) | + | |
- | - Prepare the SD card with the proper Linux image (see [[:resources:tools-software:linux-software:zynq_images|here]] and pay attention to the Linux/Windows setup), BOOT.BIN, and devicetree (you get the last ones from the previous steps) | + | |
- Insert the SD-CARD into the SD Card Interface Connector (J12) | - Insert the SD-CARD into the SD Card Interface Connector (J12) | ||
- Plug the AD-FMCOMMS2-EBZ or AD-FMCOMMS3-EBZ into the LPC Connector (J1) | - Plug the AD-FMCOMMS2-EBZ or AD-FMCOMMS3-EBZ into the LPC Connector (J1) | ||
Line 75: | Line 72: | ||
- Wait another ~30 seconds for the HDMI display device to start showing signs of life. (Linux TUX top left) | - Wait another ~30 seconds for the HDMI display device to start showing signs of life. (Linux TUX top left) | ||
- Follow the instructions for the type of demo that you want to do on screen. | - Follow the instructions for the type of demo that you want to do on screen. | ||
+ | |||
+ | <note tip> | ||
+ | If you want to manually build the HDL project and make the BOOT.BIN, see [[:resources:fpga:docs:build|this tutorial]]. For the Zynq Linux kernel and the devicetree, check [[:resources:tools-software:linux-build:generic:zynq|this tutorial]]. | ||
+ | </note> | ||
Setup/Wiring. (click to enlarge): | Setup/Wiring. (click to enlarge): | ||
Line 81: | Line 82: | ||
**Note:** For proper robustness shield the ZED board with a plexi-glass cover. Add a "Touch-Screw" (A2, stainless steel) and connect it via a 270kOhm resistor to a GND pin. Touch this screw prior any handling of any board. It ensures proper and painless ESD discharge. | **Note:** For proper robustness shield the ZED board with a plexi-glass cover. Add a "Touch-Screw" (A2, stainless steel) and connect it via a 270kOhm resistor to a GND pin. Touch this screw prior any handling of any board. It ensures proper and painless ESD discharge. | ||
- | |||
- | |||