Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:ad-fmcomms2-ebz:hardware [25 Nov 2015 14:42] – old revision restored (25 Mar 2014 21:27) Lars-Peter Clausen | resources:eval:user-guides:ad-fmcomms2-ebz:hardware [14 Oct 2016 13:30] – [Downloads] change the link for 2450BL15B050 Lucian Sin |
---|
| |
<WRAP round download 65%> | <WRAP round download 65%> |
<WRAP info>This is the latest and greatest Rev "E" of this board. Note that the Baluns on the Rev C board (T101-T104) are Johanson Technology's [[http://www.johansontechnology.com/images/stories/ip/baluns/Balun_2450BL15B050.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[./hardware/configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology's 2450BL15B050E balun. | <WRAP info>This is the latest and greatest Rev "E" of this board. Note that the Baluns on the Rev C board (T101-T104) are Johanson Technology's [[http://www.johansontechnology.com/datasheets/baluns/JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[./hardware/configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology's 2450BL15B050E balun. |
| |
</WRAP> | </WRAP> |