Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:eval:user-guides:ad-fmcomms2-ebz:hardware:configuration_options [14 Oct 2016 13:36] – [Configuration Options for AD9361 boards] change the link for 2450BL15B050E Lucian Sin | resources:eval:user-guides:ad-fmcomms2-ebz:hardware:configuration_options [24 Oct 2016 14:14] (current) – added fmcomms4/ad9364 to configuration options Lucian Sin |
---|
====== Configuration Options for AD9361 boards ====== | ====== Configuration Options for AD9361/AD9364 boards ====== |
| |
By default, the [[../|AD-FMCOMMS2-EBZ]] and [[../../arradio|ARRADIO]] board includes the Johanson Technology's [[http://www.johansontechnology.com/datasheets/baluns/JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an alternative balun should be installed. A list of alternative baluns are below: | By default, the [[../|AD-FMCOMMS2-EBZ]], [[resources/eval/user-guides/ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] and [[../../arradio|ARRADIO]] board includes the Johanson Technology's [[http://www.johansontechnology.com/datasheets/baluns/JTI_Balun-2450BL15B050_12-03.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an alternative balun should be installed. A list of alternative baluns are below: |
| |
===== Receive Balun ===== | ===== Receive Balun ===== |