This version (10 Jun 2019 03:04) was approved by erbe reyta.
Production testing of the AD-FMCOMMS11
Overview
The production testing is quite simple. Since each board has been completely characterized, and we know the layout is good, we can just look for gross errors.
There are multiple ways to run the test depending on the hardware setup.
The test parameters limits are stored in a “csv” file which can be specified in the arguments when running the console test binary. The GUI version uses the test parameters limits stored in the BOOT partition.
Requirement
Preparing the SD Card
If you have a production test SD-card already, you can skip this section and proceed to the Hardware Setup section.
Obtain the pre-built SD card Zynq image for ZC706 pre-installed with the fmcomms11 test program from this link. If the image file is compressed – that is, not ending with “.img” but with file extensions of xz, zip, and rar, decompress the file using 7zip or similar tool. Insert the SD card (at least 8gb ) to a computer. Using a disk writer software, write the downloaded image (img file) to the SD card. Instructions can be found on https://wiki.analog.com/resources/tools-software/linux-software/zynq_images/windows_hosts about how to use the Win32 disk manager. Etcher, on the other hand, is easier to use than win32 disk manager.
Example Disk writer software:
Once the image has been written on the SD card, it is now ready to use. Eject the SD card from the card reader and proceed to the hardware setup.
Hardware Setup
Plug in the external monitor and connect it via HDMI to the carrier board.
Connect the
USB OTG adapter (and
USB hub if needed) to the
USB port on the carrier, then plug in the keyboard and mouse as well.
Attach the FMCOMMS11 that has a hardware loopback to the Carrier board via the FMC HPC connector (J37).
Attach the power supply cable of the fan to the fan supply cable connected to J61. Make sure that the fan is attached to the FMCOMMS11 securely.
Insert the
SD card that contains the Zynq image and confirm that the carrier board is set to boot from
SD. The SW11 is configured the same as the following image to ensure that the carrier will boot from
SD card.
Software Setup
If the Zynq image used is the pre-built image pre-installed with the test program, there is no other software setup needed.
Test process
Make sure that Zynq Carrier board is turned-off during each start of the test.
Attach the RF loopback cable to the card. See the image in the Hardware Setup section for correct placement.
Attach the card into the carrier board through the FMC HPC J37.
Power on the carrier board.
A terminal window open and a dialog box will prompt with a message ensuring that the loopback cable is connected as instructed in step 2. Click OK if the RF loopback cable is already connected. If there is no dialog box, double-click the FMCOMMS11 Test icon in the desktop.

When prompted with a window like the following image, enter the serial number found on the board. Pressing cancel will just cancel the test.

After entering the serial number, the test will start, and progress will be shown on the terminal.

When tests pass, the following window should be shown

If tests fail, a window like the following image should be shown below. In either case, hit the OK button to end the test program. You may re-run the test software from the desktop to re-test.

In case of Program errors, the message box like the image below will appear:

The instructions on what to do with the error will be displayed on the message box. In the case above, the error might be solved by stopping all programs that are using the libiio. For example, when the IIO-Oscilloscope plot is running, this error will appear. So, stopping IIO-Oscilloscope might fix it. If the test has been restarted but the same error appears, the board under test has failed. If the next boards have the same problem, retest a board that was tested before that “passed” to check the state of the carrier board.
If test ended but did not automatically shut down, Click the icon in top left, click the log-off icon, then, click the shutdown button. During shutdown, the desktop view will exit and turn black. After several seconds power off the carrier board via the physical switch. SW1.
Once the carrier board is already powered down, remove the FMCOMMS11 that was tested and return to step 1 to continue with the next board.
In each test except for program errors, two files are generated, and a summary file will be updated.
Measurement file (f_measurement-XXXXX.csv where XXXXX is the serial number) - Contains all the data from the measurements done in the program
Processed File (f_processed-XXXXX.csv) - contains the mean, standard deviation, as well as the PASS or FAIL remarks for the individual test set.
Summary File (f_summary.csv) – contains the list of board serial numbers that has been tested and the result of most recent test on each board. Therefore, running the test again will just update the result and overwrite the processed file and measurement file of that board.
Re-running the test on the same board serial number will just overwrite the previous test results for that serial number. These files will be stored in /boot/test_results/. To backup these files, turn off the carrier board, remove the
SD card, and insert the
SD card to the computer. Locate the detected removable drive named “BOOT” and copy the test_results folder to computer. As alternative, if the carrier board is connected to the network, SSH or SCP can be used to copy the files from the ZC706 to the computer.