Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-fmcomms11-ebz:reference_hdl [10 Jun 2019 10:17]
Istvan Csomortani Minor fixes realted to lane remapping
resources:eval:user-guides:ad-fmcomms11-ebz:reference_hdl [14 Jan 2021 05:11]
Robin Getz user interwiki links
Line 3: Line 3:
 ===== Functional Overview ===== ===== Functional Overview =====
  
-The HDL reference design is an embedded system built around a processor core either ARM, NIOS-II or Microblaze. A functional block diagram of the system is shown below. The high speed digital interface of the converters is handled by the [[https://​wiki.analog.com/​resources/​fpga/​peripherals/​jesd204|JESD204B framework]]. Due to the system'​s memory interface bandwidth limitation, there are intermediary buffers in the both TX and RX data paths, in order to save and push data using high data rates. In case of the ZC706 carrier board, the RX buffer depth is 1Gbyte, and TX buffer depth is 1Mbyte. This depths can be swapped if required.+The HDL reference design is an embedded system built around a processor core either ARM, NIOS-II or Microblaze. A functional block diagram of the system is shown below. The high speed digital interface of the converters is handled by the [[/​resources/​fpga/​peripherals/​jesd204|JESD204B framework]]. Due to the system'​s memory interface bandwidth limitation, there are intermediary buffers in the both TX and RX data paths, in order to save and push data using high data rates. In case of the ZC706 carrier board, the RX buffer depth is 1Gbyte, and TX buffer depth is 1Mbyte. This depths can be swapped if required.
  
 By default the AD9162 is configured in complex mode with 8 lanes (see Table 16. in data sheet), and the AD9625 is configured in generic operation mode with 8 lanes (see Table 16. in data sheet). Both JESD204 interfaces run in Subclass 0. By default the AD9162 is configured in complex mode with 8 lanes (see Table 16. in data sheet), and the AD9625 is configured in generic operation mode with 8 lanes (see Table 16. in data sheet). Both JESD204 interfaces run in Subclass 0.
Line 417: Line 417:
 ===== Building the HDL Project ===== ===== Building the HDL Project =====
  
-When building the project, you should always use the recommended version of the tools for the specific [[https://​wiki.analog.com/​resources/​fpga/​docs/​releases | release]]. In this example, we'll use release 2019_r1, which has Vivado 2018.3 as the recommended version. If you're using different Vivado versions, it's possible that there are slight modifications on how the synthesis works, or different Xilinx IP changes, which affect the system functionality.+When building the project, you should always use the recommended version of the tools for the specific [[/​resources/​fpga/​docs/​releases | release]]. In this example, we'll use release 2019_r1, which has Vivado 2018.3 as the recommended version. If you're using different Vivado versions, it's possible that there are slight modifications on how the synthesis works, or different Xilinx IP changes, which affect the system functionality.
  
 <​code>​ <​code>​
Line 439: Line 439:
 <WRAP round help 80%> <WRAP round help 80%>
 **Questions?​** Feel free to ask your questions in EngineerZone support forums. **Questions?​** Feel free to ask your questions in EngineerZone support forums.
-  * [[https://ez.analog.com/​community/​fpga|FPGA Reference Design]]+  * [[ez>community/​fpga|FPGA Reference Design]]
 </​WRAP>​ </​WRAP>​
 ===== References ===== ===== References =====
resources/eval/user-guides/ad-fmcomms11-ebz/reference_hdl.txt · Last modified: 14 Jan 2021 05:11 by Robin Getz