This is an old revision of the document!
<WRAP round download>
For those that don't want to load up the Allegro viewer, here is a basic outline/component placements of the board. The PCB measures 100mm x 62mm and is the same form factor as the RFSOM
The size of the board (not including the SMA connectors, which project beyond the edge of the board) is 100mm x 62mm. The mounting holes align with the carrier card (AES-PZSDRCC-FMC-G), and are shown below.
The AD-PZSDR2400TDD-EB is a 4 layer board.