Wiki

This version (10 Jun 2019 03:04) was approved by erbe reyta.

AD-FMCOMMS11-EBZ Certification

Both CE and FCC are necessary for system level products.

Because ADI boards are custom built evaluation kits destined for professionals (you) to be used solely at research and development facilities for such purposes, they are considered exempt from the EU product directives and normally are not tested for CE or FCC compliance.

If you choose to use your board to transmit using an antenna, it is your responsibility to make sure that you are in compliance with all laws for the country, frequency, and power levels in which the device is used. Additionally, some countries regulate reception in certain frequency bands. Again, it is the responsibility of the user to maintain compliance with all local laws and regulations.

Navigation - AD-FMCOMMS11-EBZ

resources/eval/user-guides/ad-fmcomms11-ebz/certification.txt · Last modified: 15 Feb 2019 01:50 by erbe reyta