Wiki

This version is outdated by a newer approved version.DiffThis version (11 Nov 2022 13:43) was approved by Raluca Chis.The Previously approved version (11 Nov 2022 12:47) is available.Diff

This is an old revision of the document!


Linux on the Xilinx KC705 Kintex™-7 FPGA development Board

This guide provides some step-by-step instructions on how to build a Microblaze Linux Kernel image for the AD-FMCOMMS1 FMC board connected to an KC705.

Required Software

Latest released files can be downloaded from here

Build Linux - Step by Step instructions

Get Microblaze Little Endian Toolchain from Xilinx

The Microblaze Little Endian Toolchain can be found in the Xilinx Vitis install folder:

For 64-bit hosts use:
/opt/Xilinx/Vitis/2021.2/gnu/microblaze/linux_toolchain/lin64_le/bin

Get Linux kernel source

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1$ git clone https://github.com/analogdevicesinc/linux.git
Cloning into 'linux'...
remote: Counting objects: 2757163, done.
remote: Compressing objects: 100% (495484/495484), done.
remote: Total 2757163 (delta 2296596), reused 2687337 (delta 2234506)
Receiving objects: 100% (2757163/2757163), 782.04 MiB | 1.39 MiB/s, done.
Resolving deltas: 100% (2296596/2296596), done.
Dave@HAL9000:~/fmcomms1$

Checkout master branch

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1$ cd linux/
Dave@HAL9000:~/fmcomms1/linux$ git checkout master
Checking out files: 100% (16412/16412), done.
Branch master set up to track remote branch master from origin.
Switched to a new branch 'master'
Dave@HAL9000:~/fmcomms1/linux$

Set Environmental Variables

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1/linux$ export PATH=/opt/Xilinx/Vitis/2021.2/gnu/microblaze/linux_toolchain/lin64_le/bin:$PATH
Dave@HAL9000:~/fmcomms1/linux$ export ARCH=microblaze
Dave@HAL9000:~/fmcomms1/linux$ export CROSS_COMPILE=microblazeel-xilinx-linux-gnu-

Configure Kernel for KC705 XCOMM platform (aka FMCOMMS1)

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1/linux$ make adi_mb_defconfig
  HOSTCC  scripts/basic/fixdep
  HOSTCC  scripts/kconfig/conf.o
  SHIPPED scripts/kconfig/zconf.tab.c
  SHIPPED scripts/kconfig/zconf.lex.c
  SHIPPED scripts/kconfig/zconf.hash.c
  HOSTCC  scripts/kconfig/zconf.tab.o
  HOSTLD  scripts/kconfig/conf
#
# configuration written to .config
#
Dave@HAL9000:~/fmcomms1/linux$

Get Root File-System

Root File-system (initramfs) rootfs.cpio.gz must be placed in the root of your kernel tree.

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/linux$ wget http://wiki.analog.com/_media/resources/tools-software/linux-drivers/platforms/rootfs.cpio.gz
--2014-11-21 14:27:54--  http://wiki.analog.com/_media/resources/tools-software/linux-drivers/platforms/rootfs.cpio.gz
Resolving wiki.analog.com (wiki.analog.com)... 195.170.124.184
Connecting to wiki.analog.com (wiki.analog.com)|195.170.124.184|:80... connected.
HTTP request sent, awaiting response... 200 OK
Length: 3006465 (2.9M) [application/octet-stream]
Saving to: `rootfs.cpio.gz'

100%[===================================================================================================================================================================>] 3,006,465   75.1K/s   in 37s     

2014-11-21 14:28:32 (79.2 KB/s) - `rootfs.cpio.gz' saved [3006465/3006465]

Dave@HAL9000:~/linux$

Build kernel

The result of building the kernel is an elf file in arch/microblaze/boot named simpleImage.<dts file name> based on the dts specified.

The build process for the kernel searches in the arch/microblaze/boot/dts directory for a specified device tree file and then builds the device tree into the kernel image.

The following command shows the general format for the build target name. Note that the <dts file name> does not include the file extension “.dts”.

Dave@HAL9000:~/linux$ make simpleImage.<dts file name>

To see what device-trees for the different FPGA carrier and FMC module combination exist type:

Dave@HAL9000:~/linux$ ls -l arch/microblaze/boot/dts

This specifies any shell prompt running on the target or development host

Dave@HAL9000:~/fmcomms1/linux$ make -j5 simpleImage.kc705_fmcomms1
  CHK     include/linux/version.h
  UPD     include/linux/version.h
  HOSTCC  scripts/kallsyms
  HOSTCC  scripts/bin2c
  HOSTCC  scripts/dtc/checks.o
  CC      scripts/mod/empty.o
[--snip--]
  CP      vmlinux arch/microblaze/boot/simpleImage.kc705_fmcomms1.unstrip
  OBJCOPY arch/microblaze/boot/simpleImage.kc705_fmcomms1
  UIMAGE  arch/microblaze/boot/simpleImage.kc705_fmcomms1.ub
Image Name:   Linux-3.5.0-rc4-00817-gbf1afb2
Created:      Tue Dec 18 16:50:37 2012
Image Type:   MicroBlaze Linux Kernel Image (uncompressed)
Data Size:    6178556 Bytes = 6033.75 kB = 5.89 MB
Load Address: c0000000
Entry Point:  c0000000
  STRIP   arch/microblaze/boot/simpleImage.kc705_fmcomms1
Kernel: arch/microblaze/boot/simpleImage.kc705_fmcomms1is ready  (#1)
Dave@HAL9000:~/devel/git/staging_3$

The newly created Linux ELF file can now be loaded using the Xilinx ISE Microprocessor Debugger (XMD). Further instructions can be found here:

AD-FMCOMMS1-EBZ KC705 Quick Start Guide

More information

resources/eval/user-guides/ad-fmcomms1-ebz/software/linux/microblaze_kc705.1668170580.txt.gz · Last modified: 11 Nov 2022 13:43 by Raluca Chis