Wiki

This version is outdated by a newer approved version.DiffThis version (14 Dec 2012 16:44) was approved by Lars-Peter Clausen, Michael Hennerich, Charly El-Khoury.

This is an old revision of the document!


AD-FMCOMMS1-EBZ Calibration EEPROM Utility

Analog Devices uses six designations to inform our customers where a semiconductor product is in its life cycle. From emerging innovations to products which have been in production for twenty years, we understand that insight into life cycle status is important. Device life cycles are tracked on their individual product pages on analog.com, and should always be consulted before making any design decisions.

This particular articl/edocument/design has been retired or deprecated, which means it is no longer maintained or actively updated, even though the devices themselves may be Recommended for New Designs or in Production. This page is here for historical/reference purposes only.

NAME
       xcomm_cal - print and set EEPROM calibration data

SYNOPSIS
       xcomm_cal [-s] [-f FREQUENCY] INPUT_FILE

DESCRIPTION
	Print and set EEPROM calibration data. 
	Without option - print all calibration sets available.

	-f Target frequency in MHz

	-s Initialize device drivers with best match calibration set.
	   This option is used together with the -f option.

Download/Install

Git: https://github.com/analogdevicesinc/fmcomms1-eeprom-cal

root@linaro-ubuntu-desktop:~# git clone https://github.com/analogdevicesinc/fmcomms1-eeprom-cal.git
root@linaro-ubuntu-desktop:~# cd fmcomms1-eeprom-cal
root@linaro-ubuntu-desktop:~# make
root@linaro-ubuntu-desktop:~# make install

Find the EEPROM

Normally, the calibration EEPROM responds to I2C Slave address 0x55, but it depends on the hardware carrier, and the slot that the card is plugged into.

To find the eeprom - use the find command.

root@linaro-ubuntu-desktop:~# find /sys/ -name eeprom
/sys/devices/amba.1/41600000.i2c/i2c-1/1-0050/eeprom
/sys/devices/amba.1/41600000.i2c/i2c-1/1-0054/eeprom

It's normally the largest value. (the smaller value is the FRU eeprom).

Query best match calibration set for a given Frequency

This specifies any shell prompt running on the target

# xcomm_cal -f 2400 -s /sys/bus/i2c/devices/0-0055/eeprom

--- Best match ENTRY 1 ---
Calibration Frequency:  2400 MHz
DAC I Phase Adjust:             357
DAC Q Phase Adjust:             0
DAC I Offset:           214
DAC Q Offset:           25
DAC I Full Scale Adj:   401
DAC Q Full Scale Adj:   401
ADC I Offset:           -2
ADC Q Offset:           -34
ADC I Gain Adj: 32853
ADC Q Gain Adj: 32768

14 Dec 2012 16:43 · Lars-Peter Clausen

Navigation - AD-FMCOMMS1-EBZ

resources/eval/user-guides/ad-fmcomms1-ebz/software/linux/applications/xcomm_cal.1355499883.txt.gz · Last modified: 14 Dec 2012 16:44 by Lars-Peter Clausen