This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcomms1-ebz:hardware:configuration_options [15 Jan 2013 15:16] – add some info on the Pi Attenuation Robin Getz | resources:eval:user-guides:ad-fmcomms1-ebz:hardware:configuration_options [09 Feb 2021 16:07] (current) – add retired Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD-FMCOMMS1-EBZ Configuration Options ====== | ====== AD-FMCOMMS1-EBZ Configuration Options ====== | ||
+ | {{page>/ | ||
There is one main configuration which needs to be made during use of the [[../ | There is one main configuration which needs to be made during use of the [[../ | ||
Line 111: | Line 111: | ||
The default build of these attenuators is 0dB attenuation. (2 resistors are //Do Not Insert// and the remaining is a 0 ohm.) | The default build of these attenuators is 0dB attenuation. (2 resistors are //Do Not Insert// and the remaining is a 0 ohm.) | ||
- | {{navigation AD-FMCOMMS1-EBZ# | + |