Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-fmcomms1-ebz:hardware:configuration_options [02 Nov 2016 10:49]
Lucian Sin [Pi Attenuators] remove navigation links
resources:eval:user-guides:ad-fmcomms1-ebz:hardware:configuration_options [09 Feb 2021 16:07]
Robin Getz add retired
Line 1: Line 1:
 ====== AD-FMCOMMS1-EBZ Configuration Options ====== ====== AD-FMCOMMS1-EBZ Configuration Options ======
 +{{page>/​wiki/​common#​retired&​nofooter&​noheader}}
 There is one main configuration which needs to be made during use of the [[../​../​AD-FMCOMMS1-EBZ]] - to use or not to use the RF section. When not using the RF section of the board, the analog interface is directly to the ADC inputs and DAC outputs. (The RF section is not powered down, so it still consumes the same amount of power). There is one main configuration which needs to be made during use of the [[../​../​AD-FMCOMMS1-EBZ]] - to use or not to use the RF section. When not using the RF section of the board, the analog interface is directly to the ADC inputs and DAC outputs. (The RF section is not powered down, so it still consumes the same amount of power).
  
resources/eval/user-guides/ad-fmcomms1-ebz/hardware/configuration_options.txt · Last modified: 09 Feb 2021 16:07 by Robin Getz