Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [27 Mar 2015 11:28]
Andrei Cozma [Getting Started]
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [07 Nov 2016 09:37] (current)
Lucian Sin change zedboard links
Line 4: Line 4:
 ===== Supported Carriers ===== ===== Supported Carriers =====
  
-  * [[http://www.zedboard.org|ZedBoard]] ​+  * [[http://​zedboard.org/​product/​zedboard|ZedBoard]] ​
  
 |< 100% 100% >| |< 100% 100% >|
Line 11: Line 11:
 ===== Required Hardware ===== ===== Required Hardware =====
  
-  * AD-FMCMOTCON2-EBZ - Controller board +  * [[resources/​eval/​user-guides/​ad-fmcmotcon2-ebz/​hardware/​controller_board|AD-FMCMOTCON2-EBZ]] - Controller board 
-  * AD-DRVLV2-EBZ - Low voltage drive board +  * [[resources/​eval/​user-guides/​ad-fmcmotcon2-ebz/​hardware/​lv_board|AD-DRVLV2-EBZ]] - Low voltage drive board 
-  * AD-DYNO2-EBZ - Dynamo-meter Drive System (Optional) +  * [[resources/​eval/​user-guides/​ad-fmcmotcon2-ebz/​hardware/​dyno|AD-DYNO2-EBZ]] - Dynamo-meter Drive System (Optional) 
-  * [[http://www.zedboard.org|ZedBoard]]+  * [[http://​zedboard.org/​product/​zedboard|ZedBoard]]
   * 12V - 48V capable DC power supply   * 12V - 48V capable DC power supply
  
Line 25: Line 25:
 {{:​resources:​eval:​user-guides:​ad-fmcmotcon2-ebz:​test:​connections.jpg?​600|connections}} {{:​resources:​eval:​user-guides:​ad-fmcmotcon2-ebz:​test:​connections.jpg?​600|connections}}
   * Make sure the **Emergency Stop** switch is pressed (more information about drive board buttons [[resources/​eval/​user-guides/​ad-fmcmotcon1-ebz/​hardware/​lv_board|here]])   * Make sure the **Emergency Stop** switch is pressed (more information about drive board buttons [[resources/​eval/​user-guides/​ad-fmcmotcon1-ebz/​hardware/​lv_board|here]])
-  * Insert the DYNO sensor wire in P3 connector on the controller board with the black wire towards the FPGA. In case an encoder is used there is a one to one correspondence of the encoder'​s pins to the pins of the P3 connector.+  * Insert the DYNO sensor wire in the P3 connector on the controller board with the black wire towards the ZedBoad. In case an encoder is used there is a one to one correspondence of the encoder'​s pins to the pins of the P3 connector.
   * Insert the DYNO motor wire in the P2 connector on the Drive Board   * Insert the DYNO motor wire in the P2 connector on the Drive Board
   * Connect the power supply to the P1 connector and, if a second motor is used also on the P3 connector   * Connect the power supply to the P1 connector and, if a second motor is used also on the P3 connector
-  * Make sure the following LEDs are on:+  * Make sure the following LEDs are ON:
     * DS1, DS2, DS3 and DS4 on the Controller Board     * DS1, DS2, DS3 and DS4 on the Controller Board
     * DS1 and DS2 on the Drive Board     * DS1 and DS2 on the Drive Board
   * Insert the 5V supply in the left side of the DYNO   * Insert the 5V supply in the left side of the DYNO
   * Power on the ZedBoard   * Power on the ZedBoard
-  * After the board is programmed, in order to start the motor, the Emergency Stop switch must be released and then the **Reset** switch must be pressed for a few seconds.+  * After the ZedBoard ​is programmed, in order to start the motor, the **Emergency Stop** switch must be released and then the **Reset** switch must be pressed for a few seconds.
  
 |< 100% 100% >| |< 100% 100% >|
resources/eval/user-guides/ad-fmcmotcon2-ebz/quickstart/lv_setup_guide.1427452138.txt.gz · Last modified: 27 Mar 2015 11:28 by Andrei Cozma