This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [27 Mar 2015 11:27] Andrei Cozma [Getting Started] |
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [07 Nov 2016 09:37] (current) Lucian Sin change zedboard links |
||
---|---|---|---|
Line 4: | Line 4: | ||
===== Supported Carriers ===== | ===== Supported Carriers ===== | ||
- | * [[http://www.zedboard.org|ZedBoard]] | + | * [[http://zedboard.org/product/zedboard|ZedBoard]] |
|< 100% 100% >| | |< 100% 100% >| | ||
Line 11: | Line 11: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * AD-FMCMOTCON2-EBZ - Controller board | + | * [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/controller_board|AD-FMCMOTCON2-EBZ]] - Controller board |
- | * AD-DRVLV2-EBZ - Low voltage drive board | + | * [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/lv_board|AD-DRVLV2-EBZ]] - Low voltage drive board |
- | * AD-DYNO2-EBZ - Dynamo-meter Drive System (Optional) | + | * [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/dyno|AD-DYNO2-EBZ]] - Dynamo-meter Drive System (Optional) |
- | * [[http://www.zedboard.org|ZedBoard]] | + | * [[http://zedboard.org/product/zedboard|ZedBoard]] |
* 12V - 48V capable DC power supply | * 12V - 48V capable DC power supply | ||
Line 25: | Line 25: | ||
{{:resources:eval:user-guides:ad-fmcmotcon2-ebz:test:connections.jpg?600|connections}} | {{:resources:eval:user-guides:ad-fmcmotcon2-ebz:test:connections.jpg?600|connections}} | ||
* Make sure the **Emergency Stop** switch is pressed (more information about drive board buttons [[resources/eval/user-guides/ad-fmcmotcon1-ebz/hardware/lv_board|here]]) | * Make sure the **Emergency Stop** switch is pressed (more information about drive board buttons [[resources/eval/user-guides/ad-fmcmotcon1-ebz/hardware/lv_board|here]]) | ||
- | {{ :resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:emergency_stop.jpg?300 |Motor and Power connections }} | + | * Insert the DYNO sensor wire in the P3 connector on the controller board with the black wire towards the ZedBoad. In case an encoder is used there is a one to one correspondence of the encoder's pins to the pins of the P3 connector. |
- | * Insert the Dyno sensor wire in P3 connector on the controller board with the black wire towards the FPGA. In case an encoder is used there is a one to one correspondence of the encoder's pins to the pins of the P3 connector. | + | * Insert the DYNO motor wire in the P2 connector on the Drive Board |
- | * Insert the Dyno motor wire in the P2 connector on the Drive Board | + | |
* Connect the power supply to the P1 connector and, if a second motor is used also on the P3 connector | * Connect the power supply to the P1 connector and, if a second motor is used also on the P3 connector | ||
- | * Make sure the following LEDs are on: | + | * Make sure the following LEDs are ON: |
* DS1, DS2, DS3 and DS4 on the Controller Board | * DS1, DS2, DS3 and DS4 on the Controller Board | ||
* DS1 and DS2 on the Drive Board | * DS1 and DS2 on the Drive Board | ||
- | * Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM | + | * Insert the 5V supply in the left side of the DYNO |
- | {{ :resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:dyno_supply.png?300 |Dynamo-meter Drive System }} | + | |
* Power on the ZedBoard | * Power on the ZedBoard | ||
- | * After the board is programmed, in order to start the motor, the Emergency Stop switch must be released and then the **Reset** switch must be pressed for a few seconds. | + | * After the ZedBoard is programmed, in order to start the motor, the **Emergency Stop** switch must be released and then the **Reset** switch must be pressed for a few seconds. |
|< 100% 100% >| | |< 100% 100% >| |