Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [27 Mar 2015 11:14]
Andrei Cozma [Required Hardware]
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [07 Nov 2016 09:37] (current)
Lucian Sin change zedboard links
Line 4: Line 4:
 ===== Supported Carriers ===== ===== Supported Carriers =====
  
-  * [[http://www.zedboard.org|ZedBoard]] ​+  * [[http://​zedboard.org/​product/​zedboard|ZedBoard]] ​
  
 |< 100% 100% >| |< 100% 100% >|
Line 11: Line 11:
 ===== Required Hardware ===== ===== Required Hardware =====
  
-  * AD-FMCMOTCON2-EBZ - Controller board +  * [[resources/​eval/​user-guides/​ad-fmcmotcon2-ebz/​hardware/​controller_board|AD-FMCMOTCON2-EBZ]] - Controller board 
-  * AD-DRVLV2-EBZ - Low voltage drive board +  * [[resources/​eval/​user-guides/​ad-fmcmotcon2-ebz/​hardware/​lv_board|AD-DRVLV2-EBZ]] - Low voltage drive board 
-  * AD-DYNO2-EBZ - Dynamo-meter Drive System (Optional) +  * [[resources/​eval/​user-guides/​ad-fmcmotcon2-ebz/​hardware/​dyno|AD-DYNO2-EBZ]] - Dynamo-meter Drive System (Optional) 
-  * [[http://www.zedboard.org|ZedBoard]]+  * [[http://​zedboard.org/​product/​zedboard|ZedBoard]]
   * 12V - 48V capable DC power supply   * 12V - 48V capable DC power supply
  
Line 22: Line 22:
 ===== Getting Started ===== ===== Getting Started =====
  
-  * Connect the Low voltage drive board to the Controller board. +  * Connect the hardware as shown in the picture below 
-  * Connect the Controller + Drive boards assembly to FMC connector of the ZedBoard +{{:​resources:​eval:​user-guides:​ad-fmcmotcon2-ebz:test:connections.jpg?600|connections}} 
-  * Insert the 6 pin Hall connector into P7 - pin 1 is the empty slot of the Hall connector. In case an encoder is used there is a one to one corespondence of the encoder'​s pins to the pins of the P7 connector. +  * Make sure the **Emergency Stop** switch ​is pressed (more information about drive board buttons [[resources/​eval/​user-guides/​ad-fmcmotcon1-ebz/​hardware/​lv_board|here]]) 
-{{ :​resources:​eval:​user-guides:​ad-fmcmotcon1-ebz:hardware:hall_connector.jpg?300 |Hall connector ​}} +  * Insert the DYNO sensor wire in the P3 connector on the controller board with the black wire towards the ZedBoad. In case an encoder is used there is a one to one correspondence of the encoder'​s pins to the pins of the P3 connector
-  * Insert ​the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM +  * Insert the DYNO motor wire in the P2 connector ​on the Drive Board 
-{{ :​resources:​eval:​user-guides:​ad-fmcmotcon1-ebz:​hardware:​dyno_supply.png?​300 |Dynamo-meter Drive System }} +  * Connect ​the power supply to the P1 connector and, if a second motor is used also on the P3 connector 
-  ​Ensure that the Emergency Stop button P2 is pressed (more information about drive board buttons [[resources/​eval/​user-guides/​ad-fmcmotcon1-ebz/​hardware/​lv_board|here]]) +  * Make sure the following LEDs are ON: 
-{{ :​resources:​eval:​user-guides:​ad-fmcmotcon1-ebz:​hardware:​emergency_stop.jpg?300 |Motor and Power connections }} +    * DS1, DS2, DS3 and DS4 on the Controller Board 
-  * Insert the 3 pin motor connector ​into P1 and connect ​the lab power supply to P4 (more information about drive board connectors [[resources/​eval/​user-guides/​ad-fmcmotcon1-ebz/​hardware/​lv_board|here]]) +    * DS1 and DS2 on the Drive Board 
-{{ :resources:​eval:​user-guides:​ad-fmcmotcon1-ebz:​hardware:​motor_power_connections.jpg?​300 |Motor ​and Power connections }}+  * Insert the 5V supply in the left side of the DYNO
   * Power on the ZedBoard   * Power on the ZedBoard
-  * After the board is programmed, in order to start the motor, the Emergency Stop button P2 must be released and then the Reset switch ​S1 must be pressed for a few seconds.+  * After the ZedBoard ​is programmed, in order to start the motor, the **Emergency Stop** switch ​must be released and then the **Reset** switch must be pressed for a few seconds.
  
 |< 100% 100% >| |< 100% 100% >|
 ^  ^ ^  ^
  
-{{navigation AD-FMCMOTCON21-EBZ#​none#​..:​|Overview#​zynq|Linux on ZYNQ}}+{{navigation AD-FMCMOTCON2-EBZ#​none#​..:​|Overview#​zynq|Linux on ZYNQ}}
resources/eval/user-guides/ad-fmcmotcon2-ebz/quickstart/lv_setup_guide.1427451290.txt.gz · Last modified: 27 Mar 2015 11:14 by Andrei Cozma