This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [30 Mar 2015 14:31] Andrei Cozma |
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [07 Nov 2016 09:37] Lucian Sin change zedboard links |
||
---|---|---|---|
Line 4: | Line 4: | ||
===== Supported Carriers ===== | ===== Supported Carriers ===== | ||
- | * [[http://www.zedboard.org|ZedBoard]] | + | * [[http://zedboard.org/product/zedboard|ZedBoard]] |
|< 100% 100% >| | |< 100% 100% >| | ||
Line 14: | Line 14: | ||
* [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/lv_board|AD-DRVLV2-EBZ]] - Low voltage drive board | * [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/lv_board|AD-DRVLV2-EBZ]] - Low voltage drive board | ||
* [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/dyno|AD-DYNO2-EBZ]] - Dynamo-meter Drive System (Optional) | * [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/dyno|AD-DYNO2-EBZ]] - Dynamo-meter Drive System (Optional) | ||
- | * [[http://www.zedboard.org|ZedBoard]] | + | * [[http://zedboard.org/product/zedboard|ZedBoard]] |
* 12V - 48V capable DC power supply | * 12V - 48V capable DC power supply | ||
Line 33: | Line 33: | ||
* Insert the 5V supply in the left side of the DYNO | * Insert the 5V supply in the left side of the DYNO | ||
* Power on the ZedBoard | * Power on the ZedBoard | ||
- | * After the ZedBoard is programmed, in order to start the motor, the Emergency Stop switch must be released and then the **Reset** switch must be pressed for a few seconds. | + | * After the ZedBoard is programmed, in order to start the motor, the **Emergency Stop** switch must be released and then the **Reset** switch must be pressed for a few seconds. |
|< 100% 100% >| | |< 100% 100% >| |