Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Next revision Both sides next revision
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [27 Mar 2015 11:28]
Andrei Cozma [Getting Started]
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [27 May 2015 04:35]
Nick Hartl [Required Hardware]
Line 9: Line 9:
 ^  ^ ^  ^
  
-===== Required Hardware =====+===== Required Hardware =====Test
  
-  * AD-FMCMOTCON2-EBZ - Controller board +  * [[resources/​eval/​user-guides/​ad-fmcmotcon2-ebz/​hardware/​controller_board|AD-FMCMOTCON2-EBZ]] - Controller board 
-  * AD-DRVLV2-EBZ - Low voltage drive board +  * [[resources/​eval/​user-guides/​ad-fmcmotcon2-ebz/​hardware/​lv_board|AD-DRVLV2-EBZ]] - Low voltage drive board 
-  * AD-DYNO2-EBZ - Dynamo-meter Drive System (Optional)+  * [[resources/​eval/​user-guides/​ad-fmcmotcon2-ebz/​hardware/​dyno|AD-DYNO2-EBZ]] - Dynamo-meter Drive System (Optional)
   * [[http://​www.zedboard.org|ZedBoard]]   * [[http://​www.zedboard.org|ZedBoard]]
   * 12V - 48V capable DC power supply   * 12V - 48V capable DC power supply
Line 25: Line 25:
 {{:​resources:​eval:​user-guides:​ad-fmcmotcon2-ebz:​test:​connections.jpg?​600|connections}} {{:​resources:​eval:​user-guides:​ad-fmcmotcon2-ebz:​test:​connections.jpg?​600|connections}}
   * Make sure the **Emergency Stop** switch is pressed (more information about drive board buttons [[resources/​eval/​user-guides/​ad-fmcmotcon1-ebz/​hardware/​lv_board|here]])   * Make sure the **Emergency Stop** switch is pressed (more information about drive board buttons [[resources/​eval/​user-guides/​ad-fmcmotcon1-ebz/​hardware/​lv_board|here]])
-  * Insert the DYNO sensor wire in P3 connector on the controller board with the black wire towards the FPGA. In case an encoder is used there is a one to one correspondence of the encoder'​s pins to the pins of the P3 connector.+  * Insert the DYNO sensor wire in the P3 connector on the controller board with the black wire towards the ZedBoad. In case an encoder is used there is a one to one correspondence of the encoder'​s pins to the pins of the P3 connector.
   * Insert the DYNO motor wire in the P2 connector on the Drive Board   * Insert the DYNO motor wire in the P2 connector on the Drive Board
   * Connect the power supply to the P1 connector and, if a second motor is used also on the P3 connector   * Connect the power supply to the P1 connector and, if a second motor is used also on the P3 connector
-  * Make sure the following LEDs are on:+  * Make sure the following LEDs are ON:
     * DS1, DS2, DS3 and DS4 on the Controller Board     * DS1, DS2, DS3 and DS4 on the Controller Board
     * DS1 and DS2 on the Drive Board     * DS1 and DS2 on the Drive Board
   * Insert the 5V supply in the left side of the DYNO   * Insert the 5V supply in the left side of the DYNO
   * Power on the ZedBoard   * Power on the ZedBoard
-  * After the board is programmed, in order to start the motor, the Emergency Stop switch must be released and then the **Reset** switch must be pressed for a few seconds.+  * After the ZedBoard ​is programmed, in order to start the motor, the **Emergency Stop** switch must be released and then the **Reset** switch must be pressed for a few seconds.
  
 |< 100% 100% >| |< 100% 100% >|
resources/eval/user-guides/ad-fmcmotcon2-ebz/quickstart/lv_setup_guide.txt · Last modified: 07 Nov 2016 09:37 by Lucian Sin