This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [27 Mar 2015 11:14] – [Required Hardware] Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [27 Mar 2015 11:27] – [Getting Started] Andrei Cozma | ||
---|---|---|---|
Line 22: | Line 22: | ||
===== Getting Started ===== | ===== Getting Started ===== | ||
- | * Connect the Low voltage drive board to the Controller board. | + | * Connect the hardware as shown in the picture below |
- | * Connect | + | {{: |
- | * Insert the 6 pin Hall connector | + | * Make sure the **Emergency Stop** switch is pressed (more information about drive board buttons [[resources/ |
- | {{ : | + | {{ : |
+ | * Insert the Dyno sensor wire in P3 connector | ||
+ | * Insert the Dyno motor wire in the P2 connector | ||
+ | * Connect the power supply to the P1 connector and, if a second motor is used also on the P3 connector | ||
+ | * Make sure the following LEDs are on: | ||
+ | * DS1, DS2, DS3 and DS4 on the Controller Board | ||
+ | * DS1 and DS2 on the Drive Board | ||
* Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM | * Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM | ||
{{ : | {{ : | ||
- | * Ensure that the Emergency Stop button P2 is pressed (more information about drive board buttons [[resources/ | ||
- | {{ : | ||
- | * Insert the 3 pin motor connector into P1 and connect the lab power supply to P4 (more information about drive board connectors [[resources/ | ||
- | {{ : | ||
* Power on the ZedBoard | * Power on the ZedBoard | ||
- | * After the board is programmed, in order to start the motor, the Emergency Stop button P2 must be released and then the Reset switch | + | * After the board is programmed, in order to start the motor, the Emergency Stop switch |
|< 100% 100% >| | |< 100% 100% >| | ||
^ ^ | ^ ^ | ||
- | {{navigation AD-FMCMOTCON21-EBZ# | + | {{navigation AD-FMCMOTCON2-EBZ# |