Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
Next revision Both sides next revision
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [20 Feb 2015 09:32]
Andrei Cozma created
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [27 Mar 2015 11:27]
Andrei Cozma [Getting Started]
Line 11: Line 11:
 ===== Required Hardware ===== ===== Required Hardware =====
  
-  * AD-FMCMOTCON2-EBZ - Controller board. +  * AD-FMCMOTCON2-EBZ - Controller board 
-  * AD-DRVLV2-EBZ - Low voltage drive board. +  * AD-DRVLV2-EBZ - Low voltage drive board 
-  * AD-DYNO2-EBZ - Dynamo-meter Drive System (Optional).+  * AD-DYNO2-EBZ - Dynamo-meter Drive System (Optional)
   * [[http://​www.zedboard.org|ZedBoard]]   * [[http://​www.zedboard.org|ZedBoard]]
-  * 24V 3A capable ​lab power supply.+  * 12V - 48V capable ​DC power supply
  
 |< 100% 100% >| |< 100% 100% >|
Line 22: Line 22:
 ===== Getting Started ===== ===== Getting Started =====
  
-  * Connect the Low voltage drive board to the Controller board+  * Connect the hardware as shown in the picture below 
-  * Connect ​the Controller + Drive boards assembly to FMC connector of the ZedBoard +{{:​resources:​eval:​user-guides:​ad-fmcmotcon2-ebz:​test:​connections.jpg?​600|connections}} 
-  * Insert the 6 pin Hall connector ​into P7 - pin 1 is the empty slot of the Hall connector. In case an encoder is used there is a one to one corespondence ​of the encoder'​s pins to the pins of the P7 connector. +  * Make sure the **Emergency Stop** switch is pressed (more information about drive board buttons [[resources/​eval/​user-guides/​ad-fmcmotcon1-ebz/​hardware/​lv_board|here]]) 
-{{ :​resources:​eval:​user-guides:​ad-fmcmotcon1-ebz:​hardware:​hall_connector.jpg?​300 |Hall connector ​}}+{{ :​resources:​eval:​user-guides:​ad-fmcmotcon1-ebz:​hardware:​emergency_stop.jpg?​300 |Motor and Power connections }} 
 +  * Insert the Dyno sensor wire in P3 connector ​on the controller board with the black wire towards the FPGA. In case an encoder is used there is a one to one correspondence ​of the encoder'​s pins to the pins of the P3 connector. 
 +  * Insert the Dyno motor wire in the P2 connector ​on the Drive Board 
 +  * Connect the power supply to the P1 connector and, if a second motor is used also on the P3 connector 
 +  * Make sure the following LEDs are on: 
 +    * DS1, DS2, DS3 and DS4 on the Controller Board 
 +    * DS1 and DS2 on the Drive Board
   * Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM   * Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM
 {{ :​resources:​eval:​user-guides:​ad-fmcmotcon1-ebz:​hardware:​dyno_supply.png?​300 |Dynamo-meter Drive System }} {{ :​resources:​eval:​user-guides:​ad-fmcmotcon1-ebz:​hardware:​dyno_supply.png?​300 |Dynamo-meter Drive System }}
-  * Ensure that the Emergency Stop button P2 is pressed (more information about drive board buttons [[resources/​eval/​user-guides/​ad-fmcmotcon1-ebz/​hardware/​lv_board|here]]) 
-{{ :​resources:​eval:​user-guides:​ad-fmcmotcon1-ebz:​hardware:​emergency_stop.jpg?​300 |Motor and Power connections }} 
-  * Insert the 3 pin motor connector into P1 and connect the lab power supply to P4 (more information about drive board connectors [[resources/​eval/​user-guides/​ad-fmcmotcon1-ebz/​hardware/​lv_board|here]]) 
-{{ :​resources:​eval:​user-guides:​ad-fmcmotcon1-ebz:​hardware:​motor_power_connections.jpg?​300 |Motor and Power connections }} 
   * Power on the ZedBoard   * Power on the ZedBoard
-  * After the board is programmed, in order to start the motor, the Emergency Stop button P2 must be released and then the Reset switch ​S1 must be pressed for a few seconds.+  * After the board is programmed, in order to start the motor, the Emergency Stop switch ​must be released and then the **Reset** switch must be pressed for a few seconds.
  
 |< 100% 100% >| |< 100% 100% >|
 ^  ^ ^  ^
  
-{{navigation AD-FMCMOTCON21-EBZ#​none#​..:​|Overview#​zynq|Linux on ZYNQ}}+{{navigation AD-FMCMOTCON2-EBZ#​none#​..:​|Overview#​zynq|Linux on ZYNQ}}
resources/eval/user-guides/ad-fmcmotcon2-ebz/quickstart/lv_setup_guide.txt · Last modified: 07 Nov 2016 09:37 by Lucian Sin